Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
As noted on the documentation the VL53L5CX could integrate a microcontroller with an internal oscillator/PLL clock source. This could have a high frequency value in order to handle the ns-scale timing of the FlightSense technology and the histograms ...
Hello,I need to use the programmer Indart-STX with DataBlaze on a new computer but the programmer is not recognized on new windows 10/11.Where I can find the correct file to install drivers ?thanks for support,Thierry
Hi, this is my first post here so please forgive me if I'm not following some conventions.Anyway, I've encountered problem when trying to use EEPROM M24C04DRM (512kB + id page)I want to read id page address 0x00 which contains manufacturer code 0x20....
Chip select configured as Active High from tms570.SPI Frequency is 1 Mhz.
Is the modified RF-output filtering better in terms of EMI for FCC or CE-certification?The new filtering in V2 consists of two filtering stages and replaces one integrated filter 2400-2500 MHz.What is the reason for this change and why did you set ST...