Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Request product confirmation

HiThe product in the picture we attached is damaged and is about to be replaced.It is difficult to find information about the products below.Can I get the same product?Also, is this an EEPROM?Answers I'll wait.thank you.

YPark.6 by Associate
  • 803 Views
  • 3 replies
  • 0 kudos

Resolved! AS21P2TLR peak switching energy

I have a capacity of 40nF on the S2 pin, charged to a voltage of 3.3V.The D pin is at GND. The 40nF is then discharged through the analog switch. The peak current will be around 6.6A for a very short time (if the analog switch has 0.5 Ohm resistance)...

MSchi.3 by Associate
  • 549 Views
  • 1 replies
  • 1 kudos

I want to reduce the power consumed by SD card

Hi,We have designed an audio system where I have interfaced MEMs microphone and freq is 32KHz and I am storing files in the SD card. The files we record are getting stored in it in real-time so sd card is continuously in use.So, we have tested that i...

SJone.2 by Associate
  • 492 Views
  • 0 replies
  • 0 kudos

Top Marking on UFDFPN5 for M24XXX chips

What is the top marking for the following components?M24C32-FMH6TGM24C64-FMH6TGM24128-BFMH6TGThese are all UFDFPN5 packages.When marked with "4E", is that engineering samples?Is the marking "4EFT" for any of the above points?Thanks in advanced!BR,Frí...

FSigu.1 by Associate
  • 839 Views
  • 2 replies
  • 0 kudos

ST M24C02-FMC6TG

I need a formal MTBF/FIT/Reliability report for the subject PN for my product life prediction. Thanks.I need to see the FIT's at different confident levels, temperatures, ..etc. Is there a site link I can obtain the data similar your competitors offe...

TPak.1 by Associate
  • 532 Views
  • 1 replies
  • 0 kudos