Automotive MCUs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! DMEM Processor local RAM Memory configuration Issue

Micro controller : SPC584BWe tried configuring the DMEM Processor local RAM for SPC584B Microcontroller.(Attaching the DMEM Memory layout) (We have configured it outside BAF region)We tried pushing initialized global variables to this section. We hav...

JJose.4 by Associate
  • 842 Views
  • 1 replies
  • 0 kudos

How to use ICU for channels in eMOIS0 Group1 with SPC5Studio?

Hi,I am using SPC584B70E3 and I want to configure some of the inputs as an ICU. However, the SPC5Studio Limits the ICU for eMIOS0 Channels 0-7 only. I cannot configure PE[0] (eMIOS0 Channel 11 or eMIOS1 Channel 13) as ICU for instance. In the Referen...

TUyar.1 by Associate
  • 1028 Views
  • 5 replies
  • 0 kudos

UDE Workspace refers to older source files

Hello,I normally copy an old SPC5 project and paste it with an updated version number to modify the source code. But, the copied UDE workspace is referring to older source code. Can you help to fix it?Thanks in advance.Br,Sreejith

SKara.7 by Associate II
  • 521 Views
  • 4 replies
  • 0 kudos

Resolved! Issues with flash programming -SPC584Bxx

After flash programming, the program doesn't run once I disconnect the debugger and do a power cycling. Can somebody help me to find what the problem is? I use the attached build settings for Hex file generation in SPC5 Studio.

0693W00000HrSv4QAF.jpg
SKara.7 by Associate II
  • 873 Views
  • 5 replies
  • 0 kudos