Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! How to generate an hex file to use directly for download?

Hi,I'm using TMS570 with SPC5STUDIO environment.My toolchain generates out.elf and out.hex but I would like to have a byte hex stream (without address and other information) directly do use as download byanother microcontroller that lead TMS570.I hav...

Resolved! Device specific model ''SPC563M64L7'' not supported!

Posted on August 07, 2014 at 12:03Hello community, i try to use the PinMap wizard in SPC5 Studio 3 and i receive the meassage ''Device specific model ''SPC563M64L7'' not supported!'' and it seems that there is no support for any model cause i try it...

luemy by Associate
  • 1993 Views
  • 4 replies
  • 0 kudos

Bootloader via CAN SPC582B60E1

Hello All, I am currently working on implementing a bootloader via CAN on the SPC582B60E1 microcontroller (i.e., Update the firmware file using CAN). To achieve this, I have been referring to the "Firmware Updater Component" PDF document.and also ref...

SPC 58 mcu family FCCU configuration

Hi ,Based on the reference manual RM0407 {SPC58 C Line - 32 bit Power Architecture automotive MCUDual z4 cores 180 MHz, 4 MBytes Flash, HSM, ASIL-B},The following FCCU failure the user can’t inject this fault. .For more details, I also take  as a ref...

Mmechri_0-1714635412247.png Mmechri_1-1714635758861.png Mmechri_2-1714635854773.png
Mmechri by Associate
  • 1278 Views
  • 0 replies
  • 0 kudos

Resolved! SPC58ECxx C++ std::string throws linker errors

I'm working on a state machine for a console application, and I would like to use std::strings in C++, as they are much nicer to work with than C-style strings.Including the string library does not result in errors, but when I call string objects in ...

Screenshot 2024-04-19 092256.png
ajsmart by Associate
  • 2032 Views
  • 1 replies
  • 0 kudos