Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC58 performance

Hello,I created a new project using default settings only to toggle an OUTPUT just to see the microcontroller performance.I monitored that outpup with an oscilloscope and I get only 4.17MHz.I am using a SPC58NH-DISP.Is that an expected output frequen...

Resolved! Flashing directly into MCU

Hello Experts,I have AEK-MCU-SPC5LNK debugger and want to flash .hex/.out file directly into controller SPC582B.how can I do this. please share necessary step guide. I don't want to use any IDE like using debug mode to dump the code.   Waiting for re...

Resolved! DSPI parameter configuration issue of SPC5

Hello! I would like to ask what each of the three modes in the picture below represents?Also, what does it mean if the GPIO parameter is set to PORT_1? I did not see that the GPIO bit 0 for this PORT_1 port is in use in the pin configuration editor! ...

QQ图片20240515103352.png
Bwang.3 by Associate III
  • 1583 Views
  • 1 replies
  • 0 kudos

how to erase the spc560p50 Flash memory

Dear Support team, I am Nitesh kumar from HL Mando Softtech India Pvt. Ltd.     We have ADAS based project in production stage. Boot sw was already developed by Other Team. Now we want to update the boot SW using Boot Updater. But unfortunately we ar...

Resolved! Device specific model ''SPC563M64L7'' not supported!

Posted on August 07, 2014 at 12:03Hello community, i try to use the PinMap wizard in SPC5 Studio 3 and i receive the meassage ''Device specific model ''SPC563M64L7'' not supported!'' and it seems that there is no support for any model cause i try it...

luemy by Associate
  • 1915 Views
  • 4 replies
  • 0 kudos