Microcontrollers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC574S64 Crystal Confuguration

Hi I am working on SPC574S64 Controller, A20MHz Crystal is used in our boardI tried to configure it in the SPC5StudioI tried using one of the example code for the configuration where a 40MHz is used in the configuration and I tried to change to 20MHz...

_legacyfs_online_stmicro_images_0693W00000bi2xqQAA.png
VP.6 by Associate II
  • 961 Views
  • 4 replies
  • 0 kudos

SPC574S Issue with UDESTK debugger

Hi All,​I am working on SPC574S64 Controller​I am using the sample code from the SPC5 StudioPIT Time which toggles the port for 4ms, 2ms and 1ms​I have also observed one more issue with the crystal, I couldn't see the oscillation but could be my logi...

_legacyfs_online_stmicro_images_0693W00000biB6VQAU.png _legacyfs_online_stmicro_images_0693W00000biB6aQAE.png
VP.6 by Associate II
  • 401 Views
  • 0 replies
  • 0 kudos

Hello everyone, I am using a SPC584B70E5 microcontroller and I am trying to tell it a new application entry code after it wakes up from Standby Mode. Are there any methods to do it ?

I have two firmware saved into my Flash Memory at two different addresses (the former is a bootloader and the latter is my main application). After the micro is entered in Stanby Mode, I wish it would just load only my main application, skipping the ...

FCola.1 by Associate II
  • 446 Views
  • 0 replies
  • 0 kudos

Issue with UDESTK Connection with L9963E BMS board

I have a L9963E BMS development board, I have tried connecting to SPC5 UDESTK Debugger, the debugger is not getting connected (UDE STK Debugger) to the controller I have connected the power adapter and USB mini connector as well, I am using UDESTK St...

_legacyfs_online_stmicro_images_0693W00000bhccgQAA.png _legacyfs_online_stmicro_images_0693W00000bhcdeQAA.png _legacyfs_online_stmicro_images_0693W00000bhcdPQAQ.png
VP.6 by Associate II
  • 643 Views
  • 2 replies
  • 0 kudos

How to Start With Discovery Kit for SPC58NG

We want to work start on AUTOSAR domain. So, We are ordering Discovery Kit for SPC58NG Development board. We have some queries as below,This board is suitable for AUTOSAR Standards?Basic SIP is provided by ST or not along with development Board?Evolu...

SKumb.1 by Associate
  • 323 Views
  • 0 replies
  • 0 kudos

SPC5 CAN interface

Hello I'm trying to run SPC582B60 can interface. I tried if CAN_TX pin is properly set, switching it by TEST register and it works. But to get rid of all hardware problems I set can port into the loop mode. Filters are set to accept everything. I sen...

_legacyfs_online_stmicro_images_0693W00000bhrNRQAY.png _legacyfs_online_stmicro_images_0693W00000bhrPXQAY.png _legacyfs_online_stmicro_images_0693W00000bhrQQQAY.png
Rmilko by Associate
  • 1139 Views
  • 0 replies
  • 0 kudos

1}WE HAVE CONFIGURED MCR REGISTER, CTRL REGISTER AND MESSEGE BUFFER FOR NORMAL MODE. 2)WE ALSO CONFIGURED THE BIT RATE FOR 500Kbps. 3)WE DISABLED THE LOOP BACK MODE.{HERE I WAS THINKNG THE MODE WILL SHIFT INTO NORMAL MODE}

WE ARE USING SPC570S SERIES MICROCONTROLLER AND IDE TOOL-SPC5-STUDIO.WE ARE CHECKING THE OUTPUT ON CAN_H AND CAN_L PINS WITH MICROCHIP CAN BUS ANALYZER.BUT WE ARE UNABLE TO GETTING THE DATA.HERE I WAS DOING ANY THING WRONG CONFIGURATION ,COULD YOU PL...

Raghu.S by Associate
  • 419 Views
  • 1 replies
  • 0 kudos