User Activity

Hi,I am trying to communicate with BMS IC on our developed board and I donot see the communication happening with BMS IC despite of following all the instructions I have a L9963E BMS Eval board for reference,I have tapped out the SPI frames on the bu...
We have a BMS board with SPC574S64 Controller and L9963E as BMS ICI am trying to communicate with the BMS IC via Direct/Normal SPI modeI have done the necessary HW connections properly and ensured the SPI lines are proper.I am trying to communicate w...
We have a BMS board with SPC574S64 Controller and L9963E as BMS ICI am trying to communicate with the BMS IC via Direct/Normal SPI modeI have done the necessary HW connections properly and ensured the SPI lines are proper.Now I have a question:1. the...
Hi TeamI am trying to communicate SPC574 with L9963E BMS ICCan any one help in updating the CRC calculation for itI tried some simple calculation with polynomial , but I dont see any response from the BMS IC#define CRC_POLY (uint64_t)0x00000000000000...
Hi All,​I am working on SPC574S64 Controller​I am using the sample code from the SPC5 StudioPIT Time which toggles the port for 4ms, 2ms and 1ms​I have also observed one more issue with the crystal, I couldn't see the oscillation but could be my logi...