Automotive MCUs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Is SPE module discontinued for SPC58NN84E7?

Currently there is no appropriate documentation regarding the SPE module in the GTM. Is it discontinued? If anyone has a any good example regarding the SPE implementation or any application note regarding SPE. It would be helpful. 

vallabhd by Associate II
  • 203 Views
  • 3 replies
  • 1 kudos

SPI with Very Strong Drive on SPC572L64

We used to have that working but now can only used weak or medium drive on the SPI pins (SCK & SOUT).Pin mapper or manual editing of the board.c file only gives us weak (0) or medium drive(1){(int16_t)MSCR_IO_INDEX(PORT_D, SCK_4), PAL_LOW, (iomode_t)...

Larsa by Associate III
  • 420 Views
  • 2 replies
  • 0 kudos

How to use saradc with SPC570S

HelloI intend to use SARADC with SPC570S-DISP chip and I'm not able to operate correctly.I configured the saradc driver to use the pin ANP8, which corresponds to the board's potentiometer. I set up an interrupt to read the value. While the counter in...

SasukE15_0-1741165133376.png SasukE15_1-1741165185000.png
SasukE15 by Associate
  • 252 Views
  • 1 replies
  • 0 kudos

Resolved! Newbie Tutorials

Good day ST community! I am a newbie in microcontrollers and only used arduino boards so far. I am looking for tutorials and manuals for fabricating a SPC570S40E1 microcontroller board and program it using  SPC5-UDESTK. I opened this case to the ST o...

Resolved! Help me for reading and write SPC570s

Hi, MY name is Metropolis and search support for reading and write this mcu. Mcu is spc570s, i'm search information on web and not have find. Thanks for you support, i'm search Data sheet correct and tools for reading and write. King Regard

Resolved! Stellar Studio CAN Filters

Hi ! We are using an SR5E1E7 with StellarStudio. But we are struggling with CAN filters. How to setup the CAN device so it can accept any CAN-ID? Or better, how mask work for the CAN Filters ? We are using CanOpen and we can't really set every ID we ...

sacha_0-1743524208706.png
sacha by Associate II
  • 151 Views
  • 1 replies
  • 0 kudos

Unable to connect Debug_JTAG

Hi,I'm unable to connect to JTAG to debug the ECU after having successfully flashed via JTAG.Getting a message "Debug port fail" --> attached screenshot for more info.I would appreciate any insight into the potential causes of this failure. Thank you...

SPC560P34L1 Data Flash Write

Hello I want to program the data flash in the SPC560P34L1 microcontroller.  The user's manual says that double-word (64 bits) data page programming is supported, but an errata, DocID024694 Rev 4 (SPC560P34x, SPC560P40x devices errata JTAG_ID=0x2AE2_2...