Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! GetCoreID with SR5E1

I'm developing Autosar OS for multicore project for SR5E1 MCUOS needs to know which core is running.But I can't find any register which contain this infomation.Anyone know how can I GetCoreId with SR5E1 MCU?

phuongle by Associate
  • 3878 Views
  • 5 replies
  • 0 kudos

Resolved! The high level voltage of the pin

Hi, I am currently using the SPC58EC series of microcontrollers. I would like to know, for an I/O (configured in input mode), at what input voltage level it will be recognized as a high level. Is this voltage value configurable? Thank you for your re...

Resolved! SPC58EC-DISP not recognized by device manager

Hi. I have a problem when trying to establish a serial communication from SPC58 to my PC. My device manager only shows SPC58EC-DISP in the "other devices" section. 1.  SPC58EC-DISP is connected with USB cable to my PC. 2. I have installed the drivers...

Resolved! SPC5Studio Hightec pro license import problem

Hello, I am currently developing with SPC5Studio 6.0.0.In my project, I need the HighTec Pro option, so I downloaded the license and tool chain files from http://register.hightec-rt.com/st/spc5x.I placed the license file in both:- C:\SPC5Studio-6.0\l...

화면 캡처 2025-02-14 114104.png 화면 캡처 2025-02-14 114228.png jschoi0126_0-1739501502114.png

Resolved! SPC560P-DISP: Discovery+ evaluation board and CANFD

Hi everyone,I want to know if the microcontroller SPC560P-DISP: Discovery+ evaluation board allows me to work with CANFD. I want also to know if there is any tutorials to learn how to use it for this purpose.

Azizz by Associate III
  • 755 Views
  • 3 replies
  • 0 kudos

Check Stop reset in bootloader mode in SPC560B

I’m working on an SPC560B MCU project that includes both a bootloader and an application. The application runs without any issues. However, when running in bootloader mode, the MCU experiences repeated resets.Upon checking the RGM_FES (Reset Generati...

afra151 by Associate
  • 424 Views
  • 0 replies
  • 0 kudos

SPC58ECx set exception interrupt

Hi,   I'm learning to use it SPC58EC serial chip and have a question,when it was previously used on Arm chips, there were some exception handling interrupt functions,like Hard_Fault_Handle,this ensures easy traceability when problems arise, my questi...

SPC5 MCAN Wakeup

Hi there,I am working with a company developing an automotive control module that connects to several systems that must be able to wake up the module from STOP mode or Standby modeOne of the modules signals the wakeup request over the CAN bus, and I ...

Rusira by Associate
  • 369 Views
  • 0 replies
  • 0 kudos