Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L5CX ToF sensor issue during initialization procedure.

I try to use VL53L5CX ToF sensor with ST driver library in original version. Host MCU is ESP32 dev kit.During initialization procedure sensor returns error at step:status |= _vl53l5cx_poll_for_answer(p_dev, 4, 0, VL53L5CX_UI_CMD_STATUS, 0xff, 2);Befo...

0693W00000bhHoMQAU.jpg
ODoka.1 by Associate
  • 1467 Views
  • 1 replies
  • 0 kudos

VL53L3CX: estimating target distance from histogram

I have attached a couple of histograms from same object and from different distances. Distances are embedded in filename visible in image (top bar). Problem is peak position doesn’t change. I understand depth data is spread across three bins only. Bu...

v++ by Associate II
  • 3875 Views
  • 3 replies
  • 0 kudos

Resolved! How to do the Crosstalk compensation for VL53L1X with VL53L1X ULD

I use a glass for our VL53L1X sensor. But we found there is a crosstalk problem and have to use crosstalk compensation. We use VL53L1X ULD for our device. There are three functions about crosstalk.int8_t VL53L1X_CalibrateXtalk(uint16_t dev, uint16_t...

DSai.1 by Associate III
  • 2960 Views
  • 3 replies
  • 1 kudos

X-CUBE-TOF CubeMX Interrupt-Pin

Hello,It could be done in the code, but it would be nice to add the Interrupt-Pin configuration to the menu of the sensor(like the XShutPin). Thank you

_legacyfs_online_stmicro_images_0693W00000bhs4zQAA.png
AElgh by Associate III
  • 1081 Views
  • 1 replies
  • 0 kudos

VL53L5CX/VL53L7CX - material type recognition

In "Enhance Time-of-Flightperformance with new sensors based on the world’s first optical metasurfacetechnology " webinar it was presented simple way of materialrecognition of floor type for vacuum cleaner. could you tell me which parameterfrom "VL53...

KNawa.1 by Associate II
  • 1715 Views
  • 1 replies
  • 0 kudos