Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL6180X -- Unexplained "Waves" in Time of Flight Data

Hi there, My team and I have noticed an irregularity in our VL6180X sensor data that we do not understand. Despite having a stationary target (~75mm away), the calculated range values from the VL6 appear to "wave" over time, and do not settle into a ...

Kurt123_0-1690835562838.png Kurt123_1-1690835613360.png
Kurt-123 by Associate II
  • 4668 Views
  • 7 replies
  • 2 kudos

Resolved! VL53L4CD - Calibration Procedure and Tools

Hello,I'm working with VL53L4CD to have the distance between the board and some liquid. This distance could go from 20mm to 250mm. We want to protect the board with a glass and then do a calibration, first Offset then Crosstalk. Into the user manual,...

GCout.1 by Associate II
  • 4059 Views
  • 3 replies
  • 0 kudos

Resolved! cover glass vl53l5cx

by using the cover glass can the sensor still able detect close ranges (after calibration)

tarlan by Associate
  • 2153 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L1CB single shot fail

Hello,I'm using a VL53L1CB with X-CUBE-TOF1 but when i try to use the blocking one shot mode, i always get 0 target.If i use the blocking continuous mode, the first measure will always return 0 target and only the second measure will return a target....

nicolas by Senior II
  • 1915 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L8CH Drop in for VL53L8CX

I'd like to work with the raw histogram data from the VL53L8CH, which I don't believe the VL53L8CX has. Currently, I don't think that there's an evaluation board for the VL53L8CH, but it says it is "pin-to-pin" compatible with the VL53L8CX. Does this...

JGarrettW by Associate II
  • 4339 Views
  • 4 replies
  • 3 kudos

VL6180X

Hi ST experts,Is VL6180X comparable with TMD2635? 

STLearner by Associate III
  • 1089 Views
  • 1 replies
  • 0 kudos