Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL6180X sensor initialization SR03 setting

Hi, I was wondering what is the SR03 settings in initialization of VL6180X ToF sensor? I had gone through the user manual & application note AN4545 but i couldn't get the answer. If someone knows please explain. It just for educational purpose only.T...

AK_19 by Associate
  • 2528 Views
  • 1 replies
  • 0 kudos

Resolved! Something Wrong with Calibration of VL53L3CX

Vl53l3CX works well when i init it with DataInit and StartMeasurement Function,but when i add a OffsetCalibration to its init sequence,it output a distance of 8191 mm,which is obviously wrong .Paraments of calabration function are shown in the  follo...

屏幕截图 2023-10-08 155108.png 屏幕截图 2023-10-08 154035.png 屏幕截图 2023-10-08 154127.png 屏幕截图 2023-10-08 154900.png
LOMO by Associate III
  • 1544 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L5CX offline

I purchased X-NUCLEO-53L5A1 and NUCLEO-F401RE board. I assembled them and followed the Quick start guide X-NUCLEO-53L5A1 manual. I can't connect the device in the VL53L5CX. I update firmware and ST-Link before. I connected to the ST COM port via term...

JVane.1 by Associate II
  • 7766 Views
  • 6 replies
  • 0 kudos

Resolved! VL53l0x I cannot measure more than 400mm

Dear Sir,     I am trying to read the distance from the VL53Lox i can read upto 400mm , when i try to measure more the 400mm it is not reading proper reading. Please guide 

Yusuf1 by Associate
  • 2468 Views
  • 2 replies
  • 0 kudos

Resolved! Disabling VL53L5CX Autocalibration?

Hi there!​I was wondering, for a school project, if it is possible to disable te autocalibration on the VL53L5CX and if it would be possible to manually calibrate it?​Thanks! :fox_face:

TVos.1 by Associate
  • 2270 Views
  • 3 replies
  • 0 kudos

VL53L7CX_ResultsData interleaving & format

The ULD driver VL53L7CX_ResultsData object type contains range data from the VL53L7CX.  Each member that holds data for multiple zones and targets is organized in an array.Items signal_per_spad, range_sigma_mm, distance_mm, reflectance & target_statu...

VL53L3 integration time

I want to know whether the calculation of integration time using kcps and signal peak count is correct or not Signal = 3.83 kcps/spad (3.83*1000*211(SPAD ea ))/2099  =385    =>  1/385 = 2.6 ms Ambient & signal kcps, is the integration time the same?...

WJLO_0-1690975033577.png
WJLO by Associate II
  • 2586 Views
  • 3 replies
  • 0 kudos

Controling INT PIN on VL53L7CX

Hi everyone!I have a not conventional question to this device. INT pin is used in library to send interrupt to MCU. In my case i use just necessary part of library so the INT pin is not used at all.So now the question. Is it possible to use it now th...

MŻbik.1 by Associate II
  • 2400 Views
  • 3 replies
  • 0 kudos

Resolved! issue during VL53L1X crosstalk calibration

Dear Sir, We are currently in the process of conducting crosstalk calibration using the VL53L1X ultra-lite driver, but unfortunately, the results we're obtaining are not as expected. Our approach involves utilizing an A4-sized gray chart board as the...

DSai.1 by Associate III
  • 3708 Views
  • 4 replies
  • 2 kudos