Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L1X Distance Sensor 50% failure rate (erratic measurements).

Hi,We have an issue with a production build of a VL53L1X based design. The VL53L1X is interfaced to a PIC18F micro, I have inherited the codebase and hardware. The initial production run was for 500 units, of these approx 260 passed our production te...

Aurelius by Associate II
  • 9905 Views
  • 14 replies
  • 1 kudos

Resolved! VL53L8CX no I2C connection

I have a VL53L8CX time of flight sensor connected via I2C on a custom board. The Board has other devices that can talk on I2C no problem. now i cant see the i2c address of the ToF device. from my understanding everything seems to be fine and in accor...

AA.16 by Associate III
  • 2278 Views
  • 1 replies
  • 1 kudos

VL53L5CX initialization fails with ULD driver v1.3.6

I tried using VL53L5CX with ULD API v1.3.6 with an ESP32-S3. I successfully ported the base C function for I2C, as I can talk with the sensor during the first part of the initialization process. Unfortunately, when I reach the NVM part, the function ...

0693W00000YA8JvQAL.png

Resolved! VL53L5CX data is never ready

Hello !I'm working on the VL53L5CX sensor with a Nucleo L432KC.Using the ST example, and after succeeded the initialization of the VL53L5CX, the sensor's data are never ready. In the following function, the p_dev->temp_buffer[1:4] are all equals to 0...

CPoisson by Associate III
  • 3127 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L5CX arduino mega 2560

I just purchased the VL53L5CX-SATEL Breakout Boards for VL53L5CXhttps://estore.st.com/en/vl53l5cx-satel-cpn.htmland i have been trying unsuccessfully to get it to work with an Arduino Mega 2560. Does anyone know if it is possible to get it working wi...

rfashanu by Associate
  • 2015 Views
  • 1 replies
  • 3 kudos

Resolved! VL53L1X Duribility

I have been testing with the VL53L1X TOF sensor and am curious on the durability of the sensor in rugged environments. Such places would look like an industrial environment where vibration and impacts in inevitable. The sensor PCB would be potted and...

Resolved! ToF-Sensor to detect part distance

Hello, I'm trying to use a ToF-Sensor to track the distance of metal parts (sheets, cog wheels etc.) usually in the range of 0-60cm. The thing is that I am only interested in the distance of the surface that is directly below the sensor, the center o...

Jun by Associate
  • 2416 Views
  • 1 replies
  • 1 kudos