Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L0X long range mode not working

Hi, I am currently actively debugging and working with the sensor and it shows correct measurement data when i set the profile to 'Long range' example (settings from the 'um2039' User manual).     however the sensor response for RangeDMaxMilliMeter:...

RBerk1_0-1699435927774.png
RBerk.1 by Associate III
  • 5377 Views
  • 5 replies
  • 0 kudos

Using VL53L1X outdoors: which wavelengths interfere?

Good Morning,I am interested in using the VL53L1X sensor for my application. Before proceeding with the implementation, I would like to gather some information regarding the optical interferences that may affect the sensor's performance.Firstly, I am...

mikimat by Associate
  • 2452 Views
  • 1 replies
  • 1 kudos

Resolved! VL53l1X - can I fix used number of SPAD's

I use a VL53l1X looking trough a oil layer of ca. 20 mm. When getting measured distance 3 times with GetResult(), it returns (example):Status = 0, dist = 11, Ambient = 16, Signal = 20936, #ofSpads = 6Status = 0, dist = 19, Ambient = 8, Signal = 18104...

MBaum.7 by Associate III
  • 1677 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L0X Mounting

Hi STM Team,We are using VL53L0CXV0DH Sensor for our Object Detection Application in Medical Field. The Sensor is working fine, but after 1 month of time the dust in the environment covers the sensor's LED part, so, the dust was affected the overall ...

rkuma.21 by Associate III
  • 1546 Views
  • 1 replies
  • 1 kudos

Water level sensing with some challenges

I'm working on a project that requires liquid level sensing with a couple of complications I'm trying to address. The application is measuring levels in a vessel that is about 1.4m tall, so the ranges of interest are about 100mm to 1.5m. The target l...

Zandr by Associate
  • 2491 Views
  • 2 replies
  • 1 kudos

Resolved! Using VL53L4CD with other I2C devices in the same bus

Hello folks, I am trying to adapt my product to use the new VL53L4CD sensor, replacing another SPI distance sensor that is in use.However, I only have one I2C bus available and it is already shared with other sensors and devices, such as a FRAM. The ...

FFS by Associate II
  • 8777 Views
  • 8 replies
  • 3 kudos

Resolved! Cleaning TOF sensors

Can TOF sensors such as VL53L1X and VL53L5CX be cleaned with alcohol and/or cleaning wipes or be submerged in cleaning alcohol?

Resolved! Error compiling ToF sensor drivers on Linux - VL53L4CX

I am trying to compile the drivers for the ToF sensor: VL53L4CX for an embedded Linux application. I am running Ubuntu 22.04. When I try to make the drivers I get the following error:   CONFIG_STMVL53LX=m make -C /lib/modules/`uname -r`/build M=$PWD ...

Frooney by Associate
  • 1929 Views
  • 1 replies
  • 0 kudos