Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Multizone sensor calibration buffer

Dear forum,I try to understand the bin shape of the VL53L8CX / CH sensor calibration buffer while evaluating different sensor cover and their influence on ranging. Using the example8 file from the ULD driver the shape looks more or less always the sa...

_jh by Associate II
  • 2535 Views
  • 5 replies
  • 1 kudos

Resolved! TOF VL53L5CXV0DH/1 bad detections with status 255

I’m using a VL53L5CXV0DH/1 sensor in my current setup (see pictures). The goal is to detect a ball rolling between the sensor and the background. The red box is about 12cm apart.The settings is 4x4 for speed, i also noticed that 60 is not the highest...

thumbnail_IMG_7547.jpg IMG_7543.jpg 2024_11_15_15_42_31_workspace_1.5.0_NIC_TOF_rev001_Core_Src_tof.c_STM32CubeIDE.png 2024_11_15_15_22_40_workspace_1.5.0_NIC_TOF_rev001_Core_Src_tof.c_STM32CubeIDE.png
sde c.1 by Senior II
  • 1940 Views
  • 3 replies
  • 0 kudos

Resolved! VL53L4CX: How/where to store calibration data

I need to calibrate a VL53L4CX and have been reading UM2923. The functions described do not seem to bear any obvious relationship to the functions in the STM32Cube middleware which was generated for my project, which I find confusing. I it is not cle...

VL53L3 Linear Detection of Target

Hi everyone,I know there are 25 and 35 degree detection angles of VL53L3. I am aware that this situation is a mechanical situation. But I want to make a timing gate and find people's speeds. We have submitted our product to reliability and validity t...

fafeyto_0-1730290638557.png
fafeyto by Associate II
  • 1356 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L1 calibration using water target surface

Hello again!I've been trying to measure water level using the VL53L1 sensor and reading forum posts on it, and I've gathered that RefSPAD calibration isn't really recommended anymore.From my research on the topic, I know that water reflects only 2% o...

LDMigotto by Associate II
  • 2112 Views
  • 1 replies
  • 1 kudos

Resolved! VD55G0 libcamera stack source code, per LGPL 2.1

Hello,For the vd55g0, you provide a kernel driver and device tree as source here: https://www.st.com/en/embedded-software/stsw-img505.htmlYou also provide a libcamera integration stack (STSW-IMG505_LCAM), but this is closed source, and only the libca...

Bryan1986 by Associate II
  • 1884 Views
  • 2 replies
  • 3 kudos

Resolved! Is the VL53L1CB better than the VL53L1X?

We use VL53L1X for liquid level detection purposes.We believe that the “signal-rate” needs to be high in order to accurately detect the surface of the water at a distance.We are considering the VL53L1CB as a candidate.Is the VL53L1CB a good candidate...