Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VD6283 compute IR optical power

May I ask how to convert the IR channel ADC value of VD6283TX45 to IR optical power, only the RGB channel is converted to Lux in Driver, and there is no description about this IR optical power in Datasheet. 

donfulee by Associate
  • 1385 Views
  • 1 replies
  • 0 kudos

Resolved! How to achieve greater measurement precision close to Vl53L4CD?

Greetings!When I measure objects closer than 10 mm from the VL53L4CD, the result deviates significantly from what was expected, and the result also varies significantly depending on the texture and gloss of the object.Is it possible to configure the ...

JBM by Associate II
  • 8789 Views
  • 7 replies
  • 0 kudos

Resolved! Proper VL53L1X calibration procedure

Hi ST,I wanted to validate/confirm our Calibration procedure.  When we calibrate prior to calibration we set timing budget and intermeasurement to what they are normally when our code boots up.  So,  during calibration we do the same.  Can someone pl...

will3 by Associate III
  • 1456 Views
  • 1 replies
  • 1 kudos

release note for vl53l8cx_buffers.h

The "vl53l8cx_buffers.h" file bundled with X-CUBE-TOF1 seems to have been updated several times, but I would like to know what problems have been fixed in each version. Please let me know in which document the revision notes is listed.Thank you in ad...

GECdev by Associate
  • 1410 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L4CD: Measurement and Consumption Issues

We are having issues with the VL53L4CD Time of Flight Sensor.The sensor works properly after initialization, but after some measurements it starts having problems. It either stops ranging or returns a ranging result similar or equal to the previous o...

cvlt by Associate II
  • 3636 Views
  • 3 replies
  • 1 kudos

STM32duino / X-NUCLEO-53L5A1 example doesn't work

Hello ! My environment:Windows 11Arduino IDE 2.3.2STM32 Cores    https://github.com/stm32duino/Arduino_Core_STM32/wiki/Getting-StartedLibrary                 X-NUCLEO-53L5A1   1.1.1   https://github.com/stm32duino/X-NUCLEO-53L5A1                 VL53...

kuma by Associate II
  • 1111 Views
  • 1 replies
  • 1 kudos

Resolved! VL53L4CX no wrap check failure

I'm using the VL43L4CX and with every measurement, I get the next range status: VL53LX_RANGESTATUS_RANGE_VALID_NO_WRAP_CHECK_FAILFrom the documentation, I can't find any indications of what to do in this case and how to solve it.From the code I see t...

MCesn.1 by Associate II
  • 1044 Views
  • 1 replies
  • 1 kudos

Resolved! VL53L0X enclosure/cover?

Hi, I've been developing a simple water level sensor with the VL53L0X and i'm having trouble putting it into the enclosure that is protected from the moisture. I've been mainly experimenting now, but one of my problems is mounting the sensor behind g...

WhatsApp Image 2024-11-08 at 07.55.19(3).jpeg WhatsApp Image 2024-11-08 at 07.55.19(2).jpeg WhatsApp Image 2024-11-08 at 07.55.19(1).jpeg WhatsApp Image 2024-11-08 at 07.55.19.jpeg
cyclops by Associate III
  • 5048 Views
  • 7 replies
  • 1 kudos