Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Best ToF sensor for liquid measurement

Hi!I've since given up on utilizing VL53L1X for liquid level measurement. @John E KVAM had previously reccomended me to use instead the VL53L4CD sensor for this sort of application (small recipients with water), and I plan to ship it next week. But I...

LDMigotto by Associate II
  • 2214 Views
  • 1 replies
  • 4 kudos

Resolved! VL53L1CB calibration functions

Hello ST team.I am operating the VL53L1CB sensor with zephyrRTOS, I reach distances to four meters without problems, in addition to measure distance above them (eight meters top in ideal conditions), all this in ROI.I am working with the manual UM213...

Resolved! Question about ToF VL53L8X resolution.

Hello, I'm currently working on a project with a VL53L8X sensor.When I installed this product on the ceiling, the data of adults passing by is well observed, but the data of children passing by is not. I understand that this is a physical limitation ...

sejik by Associate II
  • 1992 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L8CX LPn pin ignored

I have 5 VL53L8CX on the same I2C bus.I need to set the LPn pin HIGH of the sensor I want to change address.But the problem is that I can also change the address when LPn pin is low as well.Also I also don't know how to scan I2C addresses in only one...

1MHz by Associate
  • 1979 Views
  • 3 replies
  • 1 kudos

Resolved! STM32Duino VL53L8CX

I am trying to use Satel VL53L8 Cx over Arduino due . The library I am using is stm32duino VL53l8cx but I never get any result .Connections were as per the expamples but it did not work.Is there a library I can use for this . I have earlier used VL53...

Rituraj by Senior
  • 4663 Views
  • 3 replies
  • 0 kudos

Resolved! VL53L1 accurate up to 40cm max

I hope someone can help me with the accuracy of my VL53L1 sensor. I can’t get the sensor working accurately above 40cm. I am working on a hobby project and want to use the sensor to avoid obstacles. The board I use is not an VL53L1-SATEL. It’s from a...

janvdsar by Associate II
  • 8966 Views
  • 11 replies
  • 0 kudos

10x10 Multizone Ranging on VL53L1 GUI not working

Hi,I have an X-NUCLEO-53L1A2 and a NODE_F401RE.The VL53L1.exe GUI is unstable and frequently freezes, but I could at least perform most of my experimental measurements (including MultiZone Ranging 4x4).However, when using MultiZone 10x10 Ranging, the...

kunf_0-1731692667339.png
kunf by Associate
  • 1328 Views
  • 2 replies
  • 0 kudos

Resolved! Vl53L1X Calibration Issues

We have two VL53L1X sensors side by side. Both have gilizmo cover glass and are placed 140mm from a 8.5x11 sheet of mat grey paper. Running the calibrate offset function returns 2mm for sensor one and 6mm for sensor two. Following this the Xtalk cali...