Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! which sensor is in X-NCULEO-53L8A1

There are three types of sensor in vl53l8 family, VL53L8CA, VL53L8CH and VL53L8CX. It seems like sensor in X-NCULEO-53L8A1 is VL53L8CA, but the relevant documents and resources are very few. so what should i read as a reference? what is the diffrence...

Icanguess by Associate II
  • 1056 Views
  • 3 replies
  • 0 kudos

Need HELP getting started with VL53L5CX - Nucleo L476RG

Hello everybody!I would really appreciate if you find some time to help me with my project. I want to take distance data from VL53L5CX module, which I have connected with Nucleo L476RG board exactly as in the picture uploaded. I just want this data t...

image.png
Eriol by Associate
  • 1507 Views
  • 5 replies
  • 2 kudos

Resolved! VL53L5, data can't ready

Hardware environment: STM32F405 chip and VL53L5CX-SATEL module;Software environment: Based on the STSW-IMG023 sample code, the code is ported to KEIL5 for use;Problem description: After completing the sensor initialization (ranging frequency 10hz, ra...

Resolved! VL53L4CD non volatile address change

I am using the VL53L4CD sensor with a nucleo board by using the API provided by ST.By using the xshut pin and the API, I can change the device address.But as soon as I shut down the power or reset the sensor through xshut, its address comes back to t...

lodi12 by Associate
  • 1497 Views
  • 3 replies
  • 1 kudos

VD66GY incorrect coloring

Hi, I am using the VD66GY image sensor on the STEVAL-56G3MAI board. It is connected to an Allwinner S3 with an ISP. This is my v4l2 pipeline:media-ctl --set-v4l2 '"vd56g3 0-0010":0[fmt:SGRBG10_1X10/1120x1360]' media-ctl --set-v4l2 '"sun6i-mipi-csi2":...

sebotics by Associate
  • 827 Views
  • 2 replies
  • 0 kudos