User Activity

Currently I'm using some of the vl53l5cx api functions along with some custom code. I plan to have multiple ToFs used and noted, via o-scope, that the initialization function vl53l5cx_init (looks to be blocking code?? correct me if I'm wrong) takes a...
I am currently testing the VL53L7CX sensor(w/ vl53l5cx_api) with the STM32F7 MCU. The default resolution of 4x4, when running, would consistently return distances around 2.5 -3.0 meters with a target status code of 5 for multiple runs. I then tested ...
I'm using the example project provided for the VL53L5CX and it works fine with the default 4x4. The `vl53l5cx_init` method within the vl53l5cx_api.c is where I believed it should be configured in this section where I passed in VL53L5CX_RESOLUTION_8X8...
 I'm fairly new to embedded work and noted that the pin layout that was given for X-NUCLEO-53L5A1 was for the F401RE, which I initially tested, but when attempting to configure it with the H743ZI2 I wanted to maintain the use of the ETH and USB port ...
Kudos given to