User Activity

 Hello,I am using the VL53L8CX ToF sensor (I2C) and have encountered an issue. Currently, I’m not using a coverglass, and I have set the sensor to an 8x8 resolution with a frequency of 15 Hz.The problem is that when I run the sensor in an infinite lo...
I’ve been using the "vl53l8cx" sensor to measure distances through I2C, and I noticed that when I measure distances (between 10cm and 50cm), the values reported by the sensor are consistently half of the actual distance. For example, when the actual ...