Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Techniques for multiplexing VL53L4CX

Hi @John E KVAM ... I have seen several discussions about best way to use multiple VL53L4CX sensors, and I've appreciated your responses.  ("Every reboot is its own adventure!").  I'm currently implementing an unusual setup that has 5 of these sensor...

MGG by Associate II
  • 886 Views
  • 2 replies
  • 1 kudos

VL53L5CX Gesture Recognition Implementation on STM32N657

Dear ST Support Team,I hope this message finds you well.I am currently working on a project where I aim to implement gesture recognition using the VL53L5CX sensor. However, I noticed in the official documentation that the supported cores for gesture ...

dw1 by Associate III
  • 1129 Views
  • 2 replies
  • 1 kudos

VL53L4CX Issues

Hello Everyone,We have a custom board that utilizes 10 x VL53L4CX sensors, length of board is about 66cm. For context I am using an NRF54L15 with Zephyr. On bootup they are all configured with a different address and an attempt is made to calibrate t...

imanushev by Associate II
  • 1813 Views
  • 4 replies
  • 0 kudos

Resolved! Wide FoV of upto 120°

Hi, I'm experimenting with VL53L4ED. it suits by requirements except that is has only 18° FoV. Is there any way to increase the FoV (upto120°) using a lens may be without hampering the laser class?

VL53L5CX with Zephyr on NRF Board

Hi everyone, I have been struggling to work with VL53L5CX on my NRF board using Zephyr. I used the VL53L5CX_ULD_driver_2.0.1 API and changed the platform.cpp. So far, what my problem is as follows:Failed on the vl53l5cx_init, because after the firmwa...

osugiw_0-1752315908809.png osugiw_0-1752140817597.png
osugiw by Associate
  • 1227 Views
  • 2 replies
  • 0 kudos

Resolved! Integration Support for VD56G3 Camera Sensor with STM32N6

Hi everyone,I am currently working with the STM32N6570-DK board and would like to integrate the STEVAL-56G3MAI camera module with it. The camera's overview page mentions that it supports the STM32N6 series. However, I have been unable to locate any S...

Resolved! VL53L1X FoV Range Limitation

We have designed and shipped a water level sensor based on the VL53L1X. It works well in most situations, but we have one issue in a particularly large tank (3m tall, 2m diameter). I believe this is due to reflections in the tank. It is a black tank,...

Resolved! VL53L1X issues with reading distance

I am currently using a VL53L1X Sensor to read a distance in the range of 40cm to 130cm. I initialized the Sensor to work in the short distance mode, so the range should not be a problem. I used the VL53L1X_calibration library to get the values for of...

FlorianJaeggi_0-1752159269259.png FlorianJaeggi_1-1752159361116.png