Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How do you take VL53L1 readings with I2C?

I'd like to use a ST VL53L1 to measure distance, but am thoroughly confused by the API. It uses a standard I2C protocol per the datasheet.In lieu of instructions on how to configure and take readings, the datasheet points to a separate document: UM21...

DOCon.1 by Senior
  • 5262 Views
  • 8 replies
  • 2 kudos

Resolved! Can this product VL53L0X work in high vaccum range condition( 10^-3 to 10^-8 torr)? What is the resolution of this product VL53L0X? What is working temperature range of this product VL53L0X?

Can this product VL53L0X work in high vaccum range condition( 10^-3 to 10^-8 torr)?What is the resolution of this product VL53L0X?What is working temperature range of this product VL53L0X?

YM.2 by Associate
  • 1110 Views
  • 2 replies
  • 0 kudos

Resolved! VCNL interrupt always high

HelloI'm working on a project with VCNL4010 sensor connected to STM32.I followed the annotation note to set the VCNL ready to get an interrupt when a value is exceeded.The AN file said:Set Led current, in my case 200mASet Frecuency to proximation rat...

Kotit.1 by Associate
  • 1186 Views
  • 1 replies
  • 0 kudos

X-CUBE-TOF1 dependencies

The Release Notes for the X-CUBE-TOF1 Library mention as dependencies STM32CubeHAL F4 V1.7.12STM32CubeHAL L4 V1.13.0Where can I get these HAL libraries?My STM32Cube Package Manager is currently set to use the STM32F4 MCU Package 1.26.2.What about CPU...

DMeie.2 by Senior II
  • 1150 Views
  • 1 replies
  • 0 kudos

Connect multiple VL53L5CX on the same I2C bus of Jetson Nano

Hi, I have a jetson nano and am trying to connect multiple VL53L5CX sensors to its I2C Bus 1. Therefore, I have to update the address for the sensors. According to the documentation, I need to initially pull down all the Lpn pins for the connected se...

MMube.1 by Associate
  • 5589 Views
  • 7 replies
  • 0 kudos

Setup VL53L5 ToF

Hi, I have setup the ToF VL53L5 and started with the simple rangedetektor example in Cube IDE (I'm using the Nucleo STM32F401 board with the X-Nucleo 53L5A1). I'Ve got the message in my serial terminal, that the VL53L5 was not found at the Default I2...

BAAM by Associate
  • 1546 Views
  • 2 replies
  • 1 kudos

VL53L5 Minimum distance setting for "motion indicator"

When using the function "vl53l5cx_motion_indicator_set_distance_motion(&motion_config, min_dis, delta_dis);" One requirement is that "min_dis >=400 mm" . I followed this requirement in my program but, I moved my object in the distance range of "100-...

Yunlion by Associate II
  • 1926 Views
  • 3 replies
  • 0 kudos

Resolved! VD6283 GUI does not calculate the CCT

I have downloaded the VD6283 GUI application and everything works fine except the "Light Spectrum" panel. From the manual I can see that it should calculate the CCT based on the correlation matrix but the CCT window in the top right is always empty. ...

RChit.2 by Associate
  • 1682 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L1X ROI (FOV) adjustment question

Hi team,I want to detect an moving object using the VL53L1X sensor.However, there is a problem with the installation angle of the sensor, and we arr looking for a solution.As shown in the above figure, there is interference from a fixed object betwee...

0693W00000JMndbQAD.png 0693W00000JMneZQAT.png
JKim.42 by Associate
  • 3368 Views
  • 3 replies
  • 0 kudos