Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L5 Status code 2, when there is no target

Hello,I have connected a "VL53L5 Satel" board to my Arduino nano BLE board, with modified example code. It works fine with: distance/motion indicator in 4 x 4, continuous mode, ranging frequency 1-10 Hz ( i tried different f). But it only works fine ...

Yunlion by Associate II
  • 1533 Views
  • 2 replies
  • 0 kudos

Usage of VL53L1X for an Electronic Target System

Hi all,​I'm planning on building my own electronic target for pistol shooting - 4.5mm pellets (4.5mmx5mm approx) traveling at 500-600 fps.​I've read the documentation on the L0X and L1X but I'm struggling to figure out if these sensors can fit the bi...

PSilv.3 by Associate
  • 1694 Views
  • 2 replies
  • 0 kudos

Where is VL53L1_PRESETMODE_RANGING defined?

UM2133 says that the available modes are VL53L1_PRESETMODE_RANGING, VL53L1_PRESETMODE_MULTIZONES_SCANNING, VL53L1_PRESETMODE_LITE_RANGING (Obsolete), VL53L1_PRESETMODE_AUTONOMOUS but the only definitions I can find (in API/core/inc/vl53l1_def.h in en...

VL6180 - Interrupt triggered wihoout object ranged

Hello,I am testing the interrupt modes and I have an issue when CONFIG_GPIO_INTERRUPT_LEVEL_HIGH is set to raise the interrut when far objects are detected, but the interrupt is triggered as soon as the continuos mode is started (whit no object in fr...

Jhern.1 by Associate II
  • 985 Views
  • 1 replies
  • 0 kudos

VL6180 can not range longer than 300mm

Hello,It seems the API does not allow to range up to 600mm, why? I am ranging ok up to ~350mm.I have tried to use x3 upscaling, but error is returned when doing so by:VL6180Dev_t    myDevLong;VL6180_UpscaleSetScaling(myDevLong, 3);It seems as upScali...

0693W00000HrhAYQAZ.png
Jhern.1 by Associate II
  • 2130 Views
  • 5 replies
  • 0 kudos

How to detect gesture with VL53L5CX ?

Hello,I'm actually working with the VL53L5CX sensor, i would like to how i can implement gesturedetection like those of the VL53L0 sensor? Do i need more than one ? Is there a specific library ?Thanks for your respons.SL

Slava.1 by Associate
  • 1177 Views
  • 1 replies
  • 0 kudos

VL53L1X sensor address getting reset to 0x29 abrupty

Hi,I'm using the VL53L1X sensor with my raspberry Pi3.Using the python code to read from the two sensors. On starting changing the address using the XSHUT pin.The Pi3 is powered from a battery via regulator. The setup also has an option of being char...

AM.1344 by Associate
  • 1898 Views
  • 2 replies
  • 0 kudos

Resolved! What is the meaning of sigma in L5?

 Hi,I saw in a video (See the screenshot above) that the distance of target is extracted by assuming a normal distribution, and for L5 sensor, we can get sigma (See the second screenshot above).My question is, do the received range sigma means the si...

0693W00000HqrkxQAB.png
Yli.9 by Associate II
  • 1621 Views
  • 2 replies
  • 0 kudos