cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L1X sensorState returns 0 at bootup

HMull.1
Associate II

Hello all,

I am using the VL53L1x ultra lite driver from ST. I have 34 VL53L1X devices currently running and two of these devices suddenly would not boot the VL53L1X sensor. Note that this device did work before.

We also have a GSM modem on the board and I have noticed RF interference that affects the sensor. I have therefore opted to switch off the modem before booting the sensor. Note also the extremely long delays when toggling the XSHUT pin.

Basically, the sensorState value stays zero until the watchdog times out (after about 30s). The whole device reboots and the sequence simply repeats.

Why would these 2 sensors (out of 34 running the same firmware) behave like this?

__HAL_IWDG_RELOAD_COUNTER(&hiwdg);
  modem_off_on();//modem off
  XSHUT_GPIO_Port->ODR &= (~XSHUT_Pin);
  HAL_Delay(10000);
  XSHUT_GPIO_Port->ODR |= XSHUT_Pin;
  HAL_Delay(5000);
 
  status = VL53L1_RdByte(DEV, 0x010F, &byteData);
 
  status = VL53L1_RdByte(DEV, 0x0110, &byteData);
 
  status = VL53L1_RdWord(DEV, 0x010F, &wordData);
 
  while (sensorState == 0) {
    status = VL53L1X_BootState(DEV, &sensorState);
    HAL_Delay(2);
  
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
John E KVAM
ST Employee

That's an odd one. I have no idea.

One wonders what would happen if you ignore the BootState and simply continue.

The sensor takes under 1ms to boot, so it should be up 1ms.

So one might guess that your toggling of the XSHUT line did not go as planned.

One might check the 'status' from the return of the call to BootState. Perhaps the I2C has failed somehow?

Noise on the I2C line can case a 'bus stuck low' issue that takes down the I2C.

But that is all I can think of.

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.