Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What's the meaning of the Reference SPADs calibration? What's the meaning of the number and type of reference SPADs? What happens if VL53L0X_SetReferenceSpads() and VL53L0X_GetReferenceSpads() are not used?

I have used VL53L0X without using VL53L0X_SetReferenceSpads() and VL53L0X_GetReferenceSpads(). The VL53L0X are working well without using them. I found out that some VL53L0Xs have narrower FOV than others and that VL53L0X_SetReferenceSpads() and VL53...

WOh.2 by Associate II
  • 1124 Views
  • 1 replies
  • 0 kudos

Resolved! tap / double-tap detection using VL53L3CX

I would also like to clarify whether there is support for the multi-zone VL53L3CX sensor? Do you have code samples or libraries for tap / double-tap detection using VL53L3CX?

Vandr.1 by Associate II
  • 1392 Views
  • 1 replies
  • 0 kudos

We would like to use the VL6180 sensor in an underwater robot and we would like to know some details about the sensor in order to find the most suitable configuration for our needs.

Is it possible to adjust the LED current ? (increase the current a little bit to compensate for water absorption).Could you give us more details about the WAF? because we've observed a strange behavior during underwater measurements (for targets with...

jmont.2b by Associate
  • 1418 Views
  • 2 replies
  • 0 kudos

Is the VL53L5CX IEC 60825-1:2007 and IEC 60825-1:2014 compliant and harmonized with the DIN EN ? Is there a compliance report available ?

Hello,Next week I have to assemble and demonstrate my project in my local school. My project includes the VL53L5CX-Satel. Does the VL53L5CX compliant with the DIN EN ? Can you provide me a compliance report wich include all the measured limits of the...

MaikH by Associate II
  • 4182 Views
  • 9 replies
  • 0 kudos

Dust free advice - ToF cover glass

During "Discover our latest range of ToF sensors featuring improved short range performance"(28.06.22) it was said you have tip to reduce dust for cover glass. I want to ask about this tip.

KNawa.1 by Associate II
  • 2601 Views
  • 2 replies
  • 0 kudos

How to get proper lux readings from VD6283

I'm working on a mass market application involving VD6283.I run the VD6283 app_lux_cct, and control the sensor using a serial terminal on the PC.The 6 channels are properly displayed along with the lux and cct.However, when I increase or decrease the...

Mvan .18 by Associate II
  • 2067 Views
  • 3 replies
  • 0 kudos

VL53L5CX High current draw in HP idle.

Hello,I have a X-NUCLEO-53L5A1 board wired up with SDA, SCL, 5V, PWR_EN and GND only. The sensor works and current draw is as expected in its ranging and LP idle states. However, when first booted up it will draw a normal 6mA in its HP idle then will...

jspiller by Associate II
  • 1211 Views
  • 1 replies
  • 1 kudos