User Activity

I have used VL53L0X without using VL53L0X_SetReferenceSpads() and VL53L0X_GetReferenceSpads(). The VL53L0X are working well without using them. I found out that some VL53L0Xs have narrower FOV than others and that VL53L0X_SetReferenceSpads() and VL53...
The datasheet shows VL53L0X has 25 degrees of FOV. However each VL53L0X shows slightly different FOV.For example, one VL53L0X seems to be 24 degrees, another VL53L0X seems to be 26 degrees.What is the FOV range of VL53L0X?If possible, I hope to maxim...
Range Status value 3 is "Min Range Fail", which is checked by reading from VL53L0X_REG_RESULT_PEAK_SIGNAL_RATE_REF.What is the Peak Signal Rate Ref.?​I'm finding how to differentiate between a reflective sheet and a high gloss stainless steel like a ...
I think those two values are for HDR(High Dynamic Range). Am I right?1. If so, is it possible to use the same value for VL53L0X_VCSEL_PERIOD_PRE_RANGE and VL53L0X_VCSEL_PERIOD_FINAL_RANGE?​The amplitude(brightness) of the reflective sheet gradually l...
I understood just RangeMilliMeter and SignalRateRtnMegaCps.Could I know the details about the followings:RangeDMaxMiliMeterAmbientRateRtnMegaCpsEffectiveSpadRtnCountRangeStatus's Min Range Fail​Best Regards,Woojin
Kudos from