Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L5CX High current draw in HP idle.

Hello,I have a X-NUCLEO-53L5A1 board wired up with SDA, SCL, 5V, PWR_EN and GND only. The sensor works and current draw is as expected in its ranging and LP idle states. However, when first booted up it will draw a normal 6mA in its HP idle then will...

jspiller by Associate II
  • 1233 Views
  • 1 replies
  • 1 kudos

VL53L4CX integration with esp32 problem

I am trying to measure with the sensor VL53L4CX controlled by an ESP32 (4MB Flash) on ESP IDF. I have installed the drivers STSW-IMG029 v1.2.8 and implemented the I2C functions to read from the sensor, but the ESP32 boot when the I2C read something f...

0693W00000NsHT0QAN.png
Mcabe.1 by Associate II
  • 2905 Views
  • 3 replies
  • 0 kudos

VL53L1X minimum time to to scan from standby

I apologize I have not read ALL of the related documentation but have read enough to feel it may be hard to resolve this question:I would like to employ the VL53L1X to detect object flow, i.e. people, however as someone has already point out it requi...

Tcodd.1 by Associate II
  • 1359 Views
  • 1 replies
  • 1 kudos

VL53L1X sensor integration and stability in indoor

Hi,I am using the VL53L1X sensor interface on my MCU platform. I am able to get the data while there is an object. But the distance is not matching as per my object.Less than 20cm it is able to detect, but after that it is not giving any stable value...

Akuma.6 by Associate III
  • 2496 Views
  • 4 replies
  • 0 kudos

vl53L3cx implementing in own STM32 project

Hi,I want to implement the vl53L3cx onto my own board , using CUBEIDE , HAL driver and an STM32G473CCT6 controller.I have read dozens of documents, but it's quite overwhelming and not clear which API to use.I have now implemented this API in my proje...

sde c.1 by Senior II
  • 2871 Views
  • 4 replies
  • 0 kudos