Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L5CX less sensitive gesture recognition

I would like to make a gesture recognition to be less sensitive for my application. I know that I am able to change parameters like GW_MIN_SPEED_X_MM_S, GW_MIN_VX_ON_VY, etc, but I am not exactly sure which parameters to change and how much I need to...

SOsle.1 by Associate
  • 1477 Views
  • 1 replies
  • 0 kudos

Range Status 4 with VL53L1X

Hi ST Team,I just integrated ULD driver of VL53L1X but it keeps returning range status: 4. What could be the problem?Settings:Timing: 100Inter Measurement: 100Distance Mode: ShortROI: 16x16Signal: Default ( 1026 something )Sigma: 90The I2C communicat...

AShar.10 by Associate III
  • 5488 Views
  • 8 replies
  • 0 kudos

VL53L5CX: detects ghost object

I'm using 8 sensors to detect the object position.This image is the part of them. The result of detecting is like the attached video.It's the capture video of my application. It visualizes the angle and distance of 2 sensors.It only shows 2nd row 8 z...

0693W00000QNViTQAX.jpg 0693W00000QNVi9QAH.jpg
mdex.dev by Associate
  • 1574 Views
  • 1 replies
  • 0 kudos

Range Status 6 with VL53L1X

HiI'm getting range status 6 while I'm reading the sensor, which corresponds to (No Update) Status.Test code (kept the necessary debugging prints):int16_t getDistance(void) { int status = VL53L1_StartMeasurement(Dev); uint8_t firstTimeInterrupt ...

HHaje.1 by Associate II
  • 1713 Views
  • 2 replies
  • 0 kudos

How to work with the VL53L5CX if you don't have enough memory?

Hello,My name is Joran, and I'm a student in Belgium. My school tasked me with a project that involves the use of the VL53L5CX sensor.Aside a few other guidelines, I have to follow this rule: no use of high-level programming languages (e.g. Python) o...

JVan .7 by Associate
  • 1518 Views
  • 1 replies
  • 0 kudos

VL53L1 interrupt problem

Hello.Isn't the period of interrupt not in timing budget?When tested indoors, the period of the interrupt is the timing budget.However, when testing outdoors, the interrupt cycle is irregular.If you look at UM2133 - Rev 6 page 11, what is reported wh...

joh.5 by Associate II
  • 1219 Views
  • 1 replies
  • 0 kudos

Resolved! About driver for VL53L1X

Dear Sir, ​We will develop system with VL53L1X. Now we are going to port the driver for our Thread RTOS. There are several sample version at candidates such as STSW-IMG007, STSW-IMG009 , STSW-IMG013 and STSW-IMG032. Could you give me some advice f...

DSai.1 by Associate III
  • 1599 Views
  • 2 replies
  • 0 kudos