Subject | Author | Posted | |
---|---|---|---|
Hello, now I try some equipment control which has function that watching some fault vibration, wit...
| 2023-10-31 3:30 AM | ||
hello im struggling to find how to get font on the lcd screen with some generated font c arrays i h...
| 2023-10-30 8:14 PM | ||
Do you think is possible add a second lcd display to this evaluation board also without touch scree...
| 2023-10-30 8:18 AM | ||
Hello, I am trying to use the DFSDM module on the Nucleo-H743ZI2 board . As a minimal example, i ...
| 2023-10-30 2:22 AM | ||
Hello, I'm currently embarking on making some USB and Wireless HID/Midi devices for personal us...
| 2023-10-29 1:10 AM | ||
My question is related to the stm32u575 and bu585's board definitions in the Zephyr Project. Actual...
| 2023-10-27 2:57 PM | ||
We have received STMICROELECTRONICS SPC58EG80E5QEC0X, the Terminal Plating is Nickel/Palladium/Go...
| 2023-10-27 3:05 AM | ||
Hello MT48LC4M16A2 is avilable with STM32H735IGT6? I wonder how can I connect pins between two ch...
| 2023-10-27 12:53 AM | ||
Hello, I'd like to know if there's a way to debug a software running in bank2 of a dual bank flash...
| 2023-10-27 12:45 AM | ||
Hello, I wanted to try the AT_MASTER example with my boards but could start launch the code withou...
| 2023-10-26 6:38 AM | ||
I would like to use NUCLEO-H753ZI (STM32H753ZITxLQFP144) to do the following: ・Use ADC1 and ADC2 t...
| 2023-10-25 6:46 PM | ||
Hi friends. I am doing my projects on CubeIDE and recently I upgraded my program. After that Stm-s...
| 2023-10-20 5:25 AM | ||
Hello! I’m struggling to get a decent jpeg frame rate with both OV2640 and ov5640 using DCMI. I'm ...
| 2023-10-20 3:14 AM | ||
Hello Developers, In my product solution based on STM32L496VGTX, i am currently adding NFC DFU fe...
| 2023-10-18 8:13 PM | ||
I've generated a CubeMX project for a mass storage class device and can't seem to get the OTG_FS em...
| 2023-10-16 2:43 PM | ||
We are trying to configure TIM1 and an internal comparator to turn-off the TIM1 complimentary PW...
| 2023-10-16 7:17 AM | ||
Hi ST Team, We have an issue concerning a PWM generation. We have a MCU : STM32F303 driving dir...
| 2023-10-13 3:34 AM | ||
Hi I need to start unit testing for a STM32 project in C how can I start a the testing, Can any one...
| 2023-10-13 2:30 AM | ||
Hallo, does anybody have an Example(without HAL), how I can initialize an external Interrupt with ...
| 2023-10-11 11:59 AM | ||
I have used an example code from STM of CAN loopback mode I have used a CAN transreceiver but i'm...
| 2023-10-09 10:28 PM |