Subject | Author | Posted | |
---|---|---|---|
I'm using an STPM33 digital signal processor driven by SPI using an STM32G071KBUX microcontroller. ...
| 2023-12-01 12:10 AM | ||
Hello experts, I have a requirement to use M4 to write to flash partitions under Zephyr OS. Curren...
| 2023-11-30 9:53 AM | ||
We have one of our products failing a certification test because the radiated RF energy at 168 MHz ...
| 2023-11-30 6:54 AM | ||
RM0481 says: (I am using STM32H563) USB_ISTR.IDN is the endpoint (or channel in host mode) identif...
| 2023-11-30 4:49 AM | ||
I've come across an MCU with UID {0x210044, 0x474b500e, 0x20383736} where banks are swapped despite...
| 2023-11-28 5:44 AM | ||
Hello, I want to know if it is possible to run web browser on RTOS prefferably on FreeRTOS. I tried...
| 2023-11-28 3:40 AM | ||
Hi, I am currently using two SMT32F207 for I2C transmission (MASTER writes SLAVE). Below is my conf...
| 2023-11-26 7:31 PM | ||
Ok, 2 part question. The UART bootloader defined the "special" and "extended special" commands....
| 2023-11-20 6:10 AM | ||
I am using a STM32F767BITx LQFP208. I have to measure 12 channels. 6 channels measure the voltage a...
| 2023-11-20 6:06 AM | ||
Our product uses a STM32L452 to measure the 4-20mA loop current of an external sensor. The product ...
| 2023-11-19 7:15 PM | ||
is there a way to generate (and possibly also read)a pal composite video signal using stm32 nucleo ...
| 2023-11-19 2:58 AM | ||
Hi, I just decided to try mbed OS 6 for programming my NUCLEO-WB15CC. Compilation is successful, bu...
| 2023-11-15 8:06 AM | ||
How are parts purchased from www.avaq.com? We want to purchase the stm32 series, this one https://...
| 2023-11-14 9:43 PM | ||
Hi Everyone, I am trying to implement a SSI slave for high speed applications (up to 10Mhz) on SM...
| 2023-11-13 11:30 AM | ||
Hi, As from the title, is it possible to use the same AWD to monitor 2 channels from 2 different A...
| 2023-11-13 8:37 AM | ||
Hi there, We use the I2C peripheral of the STM32H755ZI MCU. We operate the I2C in master mode and ...
| 2023-11-10 5:28 AM | ||
Hi,
I am new to work on STM32F0 discovery board. I am Implementing the USB communication TX/RX wi...
| 2023-11-06 7:50 PM | ||
I would like to preface with the fact that I am fairly new to hardware programming and electronics ...
| 2023-11-04 9:43 AM | ||
Hi, i try to get the COM35H3P70ULC Display to work with the STM32H747L-Disco Board using a custom A...
| 2023-11-03 4:01 AM | ||
I am trying to interface the STM32H747 with a quadrature encoder-equipped motor to track linear mov...
| 2023-11-02 7:09 PM |