| Subject | Author | Posted | |
|---|---|---|---|
|
Hello, I'm trying to implement a MPU test on a STM32L496ZG MCU that will be part of some self-t...
| 2023-12-12 12:59 AM | ||
|
I have written a bootloader that is used to update the application code via a Modbus interface over...
| 2023-12-11 8:27 PM | ||
|
Hi, I'm trying to use a SMB alert on a STM32F746NGH6TR. Interestingly, the corresponding interrupt...
| 2023-12-11 6:44 AM | ||
|
I spent hours trying to figure out why my interrupt didnt work. I have to say that i didnt go with ...
| 2023-12-06 1:47 PM | ||
|
Hello, I'm currently experiencing an issue with the STM32U535 HAL library, specifically when using ...
| 2023-12-05 8:18 AM | ||
|
When I downloaded applicaton into flash, I found that it will respond my cmd code if I send cmd cod...
| 2023-12-04 12:52 AM | ||
|
Hello, I am trying to install FileX + LevelX in an stm32h7 microcontroller using a nor custom ...
| 2023-12-03 2:24 PM | ||
|
Hello, Is there an option to use with Nucleo-L152RE as Power Delivery CC line sniffer and decoder...
| 2023-12-03 1:46 PM | ||
|
When using F429 to complish the function of Ethernet, a confused phenomenon appears,message sending...
| 2023-12-01 6:01 PM | ||
|
I'm using an STPM33 digital signal processor driven by SPI using an STM32G071KBUX microcontroller. ...
| 2023-12-01 12:10 AM | ||
|
Hello experts, I have a requirement to use M4 to write to flash partitions under Zephyr OS. Curren...
| 2023-11-30 9:53 AM | ||
|
We have one of our products failing a certification test because the radiated RF energy at 168 MHz ...
| 2023-11-30 6:54 AM | ||
|
RM0481 says: (I am using STM32H563) USB_ISTR.IDN is the endpoint (or channel in host mode) identif...
| 2023-11-30 4:49 AM | ||
|
I've come across an MCU with UID {0x210044, 0x474b500e, 0x20383736} where banks are swapped despite...
| 2023-11-28 5:44 AM | ||
|
Hello, I want to know if it is possible to run web browser on RTOS prefferably on FreeRTOS. I tried...
| 2023-11-28 3:40 AM | ||
|
Hi, I am currently using two SMT32F207 for I2C transmission (MASTER writes SLAVE). Below is my conf...
| 2023-11-26 7:31 PM |