STM32H750B-DK OTG_FS Device: can't get embedded DP pullup to turn on
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-10-16 2:43 PM
I've generated a CubeMX project for a mass storage class device and can't seem to get the OTG_FS embedded pullup on DP to engage. I've enabled VBUS sensing, and can confirm that the code initially does a soft disconnect (OTG_DCTL->SDIS = 1) then a connect (OTG_DCTL->SDIS = 0), then I get a VBUS sensing break-point when I plug into a PC (confirmed that OTG_DTCL-> still is 0), but I never see the pullup engage so no enumeration.
Is it true that after the initial soft disconnect and when SDIS = 0, then the pullup should engage when VBUS appears without code intervention?
Labels:
- Labels:
-
STM32H7 Series
-
USB
0 REPLIES 0