cancel
Showing results for 
Search instead for 
Did you mean: 

Poor jpeg frame rate using DCMI (<10 fps)

MS.9
Associate III

Hello!

I’m struggling to get a decent jpeg frame rate with both OV2640 and ov5640 using DCMI. I'm getting about 10fps!

I’m using what seems to be the technique that other are using to determine when a jpeg frame has arrived.

 

 

while (1) { jpegComplete=0; HAL_DCMI_Start_DMA(&hdcmi, DCMI_MODE_SNAPSHOT, (uint32_t)picBuf, 0x8000); while (jpegComplete==0); HAL_DCMI_Stop(&hdcmi); process image in picBuf... } void HAL_DCMI_LineEventCallback(DCMI_HandleTypeDef *hdcmi) { jpegComplete=1; }

 

 

What I’m finding is that HAL_DCMI_Stop() is taking 100mSec to complete.

I get about 10fps on a 480x320 image, where jpgeg image is about 10k, which cant be right. 

So the question is, is there a 'right' way to get jpeg images using DCMI?

I using stm32H723, I’ve tried all sorts of different hacks trying to improve it, I’m sure the camera, DMA & DCMI config are right as I get decent framerates in non jpeg and it seems to align with loads of sample code that I've found. Fundamentally I think the HAL_DCMI_Stop() is the problem.

 

Thanks

Mark

0 REPLIES 0