| Subject | Author | Posted | |
|---|---|---|---|
|
I have a STM32U585 product with Trustzone enabled, Bootlock disabled and RDP level 0. I want to br...
| 2026-05-06 5:39 AM | ||
|
Hi, I would like to use MDMA to get values from ADC. I have one adc set with 6 channels, starting...
| 2026-05-06 5:10 AM | ||
|
Hi, I have a problem with a custom board, where i can not enter bootloader, on some boards... I h...
| 2026-05-06 4:52 AM | ||
|
Hi, I need to measure a 4.2V battery while my MCU's supply varies between 2.0V and 3.3V. Since VDD...
| 2026-05-05 2:38 PM | ||
|
Hello, In the reference manual rm0481 (stm32h562) in chapters 7.11.38 and 7.11.51 it is stated ...
| 2026-05-05 1:32 AM | ||
|
Hello, I am working on a project where I need to both read and write regularly into the STM32 flas...
| 2026-05-05 1:25 AM | ||
|
Hello, we have designed different boards with STM32G0B1. With our latest board we find that bo...
| 2026-05-05 1:03 AM | ||
|
When TxRSTU and RETRIG are enabled with CONT disabled, will the timer still trigger a register ...
| 2026-05-03 10:27 AM | ||
|
Hi friends, Does have processors from this family a dedicated input pin as the the input for inner...
| 2026-04-30 10:35 PM | ||
|
We are trying to do a firmware upgrade via UART to the N6 from another MCU, and having trouble gett...
| 2026-04-30 2:34 PM | ||
|
Hi, I am planning to use an STM32N6 in a project where I need a real-time clock (RTC). My goal is...
| 2026-04-29 5:43 AM | ||
|
Dear Forum, I'm using a STM32F401 and implemented the I2C as Target transmitter (Slave) answering ...
| 2026-04-27 3:38 AM | ||
|
During the initialization of STM32 UHS-I, it has an IO output of 3.3V. After initialization, it out...
| 2026-04-27 1:01 AM | ||
|
:warning: Note: The internal GPIO structure has been simplified for better conceptual understa...
| 2026-04-22 5:40 AM | ||
|
Hello, I am currently working on a schematic featuring 3x STM32H753ZIT6 MCU , and I have a few que...
| 2026-04-19 11:53 PM | ||
|
Hi, Any reason why the GBW of the OPAMP is having such a wide tolerance? Is it purely because the ...
| 2026-04-08 4:19 AM | ||
|
The boot fail light doesn't seem to function the way i would think it would. When * boot 0 == ...
| 2026-04-07 7:19 AM | ||
|
We had: An STM32H7Sx with an external flash on one XSPI port, and an external RAM on the other; ...
| 2026-03-13 8:54 AM | ||
|
Greetings,
I am working with the STM32U585RI and a sensor that asserts an interrupt on the MISO l...
| 2026-03-03 12:12 PM | ||
|
Hello everyone!
I got the following problem; I need to read from two 32bit addresses and writ...
| 2026-02-16 7:09 AM |