Hello, I am developing a USB Type C charger The development environment is as follows Hardware NUCLEO-G071RB (tested on rev C) X-NUCLEO-DRP1M1 shield Software x-cube-...
Hi,
I'm trying to get the FP-AUD-AEC1 v1.2.0 acoustic echo cancellation demo application to work. I have a NUCLEO-F446RE board, an X-NUCLEO-CCA02M2 expansion board and an X-NUCLEO-CCA01M1 expansio...
Hello everyone! I have been complaining about this for 1 week. I can't make "HAL_I2C_Slave_Seq_Transmit_IT" send data to the master, but Slave to master ACK works fine, does anyone have any advice to...
Hello to everyone, I have crereated my own STM32L452 board with battery power supply. It dosent run as expected. Sometimes I need to discharge caps and sometimes this is not helping. When it works ...
Hello, I have a custom board setup with an STM32G071GBUxN and a TCPP03-M20. I have followed this STM guide for setting it up as a DRP device. It is able to negotiate as a sink with Source on...
I'm developing firmware on a G0-family device. I've implemented a CDC-ACM device based on one of the USBX sample applications. Windows finds it, enumerates it and I can open it as a COM p...
hi all,
i am using STM32U585 controller which is having a internal UCPD controller.my requirement is to create a module which can act as host and device using USB type C. i am taking the...
Hello, I am developing a USB PD sink application on custom board with STM32G0B1VET I am using periphery UCPD2. I followed AN5418 to set up eveyrthing in CubeMX and add the specified piece...
Hello I am trying to work with Microseconds delay in my code so follow this very help full post on web POST and I configure TIMER 3 ( I have also check with all available timer ) But unfortun...
Hello is it possible for the microcontroller with USB OTG to download the program memory from the USB stick itself? In other words, change the firmware simply by connecting a USB stick with a .bin ...