After I updated ST-Link to firmware version V2J43S7 through STM32 Cube Programmer, I can't connect it to my laptop and program my STM32 F405 Feather board. I have attached the error message to this p...
Hello, I generated a project for STM32U5A9J-DK with STM32CubeIDE (v1.16.0). It doesn’t include the OctalFlash test code. So, I used the test codes in chapter "Octo-SPI FLASH in Regular-comma...
Hello ST Community, I'm encountering difficulties while attempting to connect and debug my STM32 microcontroller, and I'm seeking guidance from the community. I have erased the full chip flash ...
Hello, I have been using the same cubeIDE debugger options for several months and have not had any major issues. However i recently updated to the latest macOS 15.0 release (not necessarily the cause...
I have an L432KC and to test it, I created a simple blinking program which I uploaded via USB, which works just fine. When connecting my MCU to my external 5V power supply though, my program does not...
I am using my own custom board which is replicate of stm32f429 disc1 development board.
I replaced main mcu chip i.e stm32f429 and stlink chip from my disc1 board to my custom board. After us...
Hello, I try to build a 'PDO SINK' project on B-U585I-IOT02A and I have watched the video How to build an USBPD Sink application using the X-Cube-TCPP software pack - YouTube. Issue: After build p...
Hi I am trying to communicate between arm processor and nucleo board through uart The processor has a type b usb , to interface with computer. For the same usb I am connecting my Nucelo boa...
...From my actual understanding, this means that the COM Port is not active because SB4 and SB7 are "ON" too? Is this correct? If this is true and I have to set SB4/SB7 off. How do I set SB4 a...