User Activity

Does anyone know how to enable a timer interrupt in SCP582b?
I need help understanding the SARADC test application code. Can anyone explain to me how the code works?
Is it possible to change the white theme to a dark theme in SPC5Studio?
In the SPC582B Discovery Board (QFP64 package), I need to use CAN_6_RX and CAN_6_TX which are in the uC pin 63 and 64. But when I used the CAN Test Application, I cannot find the CAN Driver related to the CAN_6. How would I program the CAN_6 protocol...