Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! UDESTK on SPC5

I couldn't find how to add UDESTK's debug screen to my SPC5, can you suggest me the correct way ?

0693W00000GYsOyQAL.png
yakdagg by Associate II
  • 2457 Views
  • 4 replies
  • 0 kudos

How tu run "Simple TCP Echo Server Demo" in SPC58EC-DISP?

Hi community!my name is Vincenzo and I would like to ask you which are the steps that I have to follow in order to run a demo available in the Application SPC58ECxx_RLA Network Ping Test Application for DiscoveryUp to now I can ping the SPC58EC-DISP ...

VNava.1 by Associate III
  • 1640 Views
  • 2 replies
  • 0 kudos

Resolved! There exist an example for SPC58EC-DISP that I can use in order to send UDP message from SPC58EC-DISP via Ethernet without include FreeRTOS Component?

Hi community! my name is Vincenzo,I am looking, if any, for an example application that would help me understand how to send UDP messages from the SPC58EC-DISP board over Ethernet.For the moment I have found an interesting application that allows me ...

VNava.1 by Associate III
  • 1435 Views
  • 1 replies
  • 0 kudos

Watchdog after WD reset

After the watchdog does a reset and the watchdog is enabled after the reset the watchdog will not cause a reset. The watchdog is enabled and not getting serviced but a reset is not occurring. What has to be done to get the watchdog working again?

CGilm.1 by Associate
  • 1723 Views
  • 3 replies
  • 0 kudos

Resolved! Anyone know a workaround when SPC5Studio does not start?

Installed SPC5Studio on an older WIN7 laptop. When trying to start the application an icon briefly appears in the taskbar - then nothing.Error log reads "A fatal error has been detected by the Java Runtime Environment..."Updated existing JAVA runtime...

KPN1 by Associate III
  • 2218 Views
  • 3 replies
  • 0 kudos

Resolved! How can I use LIN Slave mode? (SPC58EC-Disp)

Hi, I want to use LIN communication as slave in my board.I'm using SPC5Studio, and I'm checking the example code which the SPC58ECxx_RLA LIN Test Application for Discovery.This example code is used two LIN nodes and master node ask for data to slave ...

BCHOI.1 by Associate
  • 1582 Views
  • 1 replies
  • 0 kudos