I'm loading aplication's SPC58EC DISP, and debugging, but if I change the main.c this is the 9 problens. What it's, please?Another problem is that if I change and build the project, the changes not appearin the UDESTARTERKIT.
I'm using SPC_studio programer and debuging my aplication whit PLS UDE StarterKit. It's conected and program all.But i don't is possible debug? I'ts possible debug the SPC58EE84E7 with PLS UDE Starterkit? If is possible, could you sendme example ...
Hello,below it's 9 problens, If I change the main.c and build the sisten not such the directory, I see again if only write in the main one variable for example:the SPC5studio don't creat the code.
I only had created one variable in main.cIf i change anyfing in main.c have 9 problens. We see that the project folder is only read. If I uncheck box read only in the folder , after building it's return to read only.