Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Cross compiling for SPC570Sx without SPC5Studio

Posted on June 28, 2018 at 11:20Hello,I'd like to cross-compile code without using SPC5Studio for SPC570S5E1 on a linux box, which version of gcc would I need and what flags should I use? Do I need a special toolchain for the e200z0 core?Thanks in a...

SPC58EG : Watchdog SWT example doesn't work

On SPC58EG, I try to use SWTOn SPC5 Studio6 , I use the example « SPC58xGxx_RLA SWT Test Application for Discovery »In this example, it uses the SWT2, associated to core 2When the emulator Lauterbach Trace32 is connected, the example works well - The...

MRO by Associate II
  • 929 Views
  • 0 replies
  • 0 kudos

Gerber files of Module SPC564AADPT324S

Hello,I am using 324BGA spc564a. I need the gerber files of Module SPC564AADPT324S as pcb layout design reference. Or other 324BGA spc564a board design files.Thank you!

Wqs.1 by Associate
  • 911 Views
  • 0 replies
  • 0 kudos

AMU API for SPC59NN84C3

Hi,I would like to know if it already exists a C API to use the Advanced Simulation for Calibration (ASC) Modeling Unit (AMU) integrated in the SPC58NN84C3 chip that is part of the SPC58xN family chips type. In the documentation are only present the ...

AFerr.21 by Associate
  • 1032 Views
  • 0 replies
  • 0 kudos

How compile old project of SPC58?

Good morning,I am a technician who works for a company. I have to manage different projects related to the SPC58ECxx. My problems are that I can modify the bootloader or the application but if I use the configurator and re-compile they stop working. ...

GJord.3 by Associate
  • 1938 Views
  • 2 replies
  • 0 kudos

SPC58EC80: jump from application to bootloader

Hello,I am working in SPC58EC80 demo board & developing flexray firmware.I want to jump between application & bootloader for firmware update.I want to jump to bootloader mode & update firmware while application is running.Can someone suggest solution...

RSeba.2 by Associate III
  • 1025 Views
  • 0 replies
  • 0 kudos

Resolved! Why SPC560P40 trigger swt reset?

I've been feeding dog, but sometimes it still triggered swt reset.I can get reset info from reading DES and FES register.WHY??Who can tell me the FAE or technical department e-mail in China?Or tell me the reasion?