2022-11-16 7:22 PM
I'm using the AEK-MCU-C4MLIT1 evaluation kit for testing out the SPC58 MCU's. I have managed to write, generate, and build my program but I can't figure out how to actually upload my code onto the SPC58. I am coming from the STM32 MCU family where I used Keil uVision previously. Unfortunately, this was at a previous company so I don't have access to Keil anymore. Now I am using SPC5x studio, and just can't seem to find the flash MCU or upload code button. Any help would be greatly appreciated in trying to figure this out
2022-11-17 1:11 AM
Helo,
Extract from:
The board hosts a PLS debugger/programmer and an extension connector (4x37 pins) for functional interaction across boards that are compatible with the AutoDevKit initiative. The PLS Universal Debug Engine (UDE) software is available for free download and includes a free perpetual 256 Kbyte debugging/programming license.
Best Regards.