Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Freeze at configuring ATOM 3-5

Hello,My goal is to figure out how to run 15 synchronized center aligned PWM. I am trying to configure GTM ATOM module at custom board with SPC58EE80E7 with SPC5 studio GTM component RLA. Whenever I try to enable ATOM 3, 4 or 5 MCU freeze at startup....

MBedl.1 by Associate II
  • 1348 Views
  • 0 replies
  • 1 kudos

Resolved! Why I can't set HOST_DEBUG_EN in TnDCM CR register on SR6P7G7C7? I use key 0xE0E05FE0 to unlock it, but bit doesn't change the value. External debugger is not connected.

I'm working with SR6P7G7C7 and I would like to start CoreSight trace from MCU without external tools. I configured Core0 ETM and TMC ETR, but trace doesn't start. I assume the problem is in TnDCM_CR register, I am not able to set HOST_DEBUG_EN. I use...

Resolved! SPC560P50L5 CAN Communication data rate calculation

I am trying to write a code to send CAN messages using SPC560P50L5, I am trying to get idea from the SPC5 studio CAN Example but i am having difficulty understanding how to set bit rate since i am planning to set bit rate to 50000bits/s. I have gone ...

_legacyfs_online_stmicro_images_0693W00000bkBy7QAE.png
MAli.6 by Associate II
  • 2785 Views
  • 3 replies
  • 0 kudos

Resolved! CRC Algo for BMS L9963E Chip

Hi TeamI am trying to communicate SPC574 with L9963E BMS ICCan any one help in updating the CRC calculation for itI tried some simple calculation with polynomial , but I dont see any response from the BMS IC#define CRC_POLY (uint64_t)0x00000000000000...

VP.6 by Associate II
  • 2290 Views
  • 2 replies
  • 0 kudos

Hello, when I use SPC5Studio software to program the SPC582B microcontroller, how can I set the data sent by SPI communication through SPC5Studio ?

Hello, when I use SPC5Studio software to program the SPC582B microcontroller, how can I set the data sent by SPI communication through SPC5Studio? Because I cannot find the SPI module's menu or options for setting the content of data sent in the SPC5...

Bwang.3 by Associate III
  • 1582 Views
  • 3 replies
  • 0 kudos

Resolved! Flex CAN tx problem

Hello,I am working on a SPC560P Discovery Board.I have imported test application 'SPC560Pxx RLACAN Test Application for Discovery' for FlexCAN testing. In this FlexCAN0 is used in loop back mode and it is working.But after disabling loop back mode,I ...