User Activity

I am using spc5studio and SPC58EC80E1.i import crc sample from application library.i set CRC Settings at low level Drivers component RLA - CRC-32, Polymonial seed 0x4c11db7, reset = 0xFFFFFFFFand firmware code​----------------------------------------...
hello.how to put the defined version information(32bit value) in the built image (test.hex or test.bin)?
Hello.​i use SPC5Studio tooli started import samples from application library / Bootloader ...the project complie is ok.i modified Makefile. i know this file automatically generatedbut i must modify the compile option"HEX = $(U_GHS_PATH)gsrec -hex38...
i use SPC58EC80E1if feature : flash size 4MB​the flash Consisted of low block, lager block, high block.I want to write 4byte for low block (0xfc0000) in test1_func().continuously, I want to write 4byte for low block (0xfc0004) in test2_func() For exa...
Hello,i use spc58ec80e1 in our project. (spc5studio)the bootloader code is flashed in address 0x00fc0000 (Boot Mode : copy in flash),and application code is flashed in address 0x01000000.(Boot Mode : Excute from flash)After the bootloader starts to o...
Kudos from