I have data which i need to store in eeprom,but i am facing following issue:The data once written to one block of flash, not able to overwrite the dataThe other blocks not able to use during run time
I need help to develop SPC560P40 CAN driver as the examples given for that is complex and difficult to understand .Is any other document or examples code available, which is simple or uses register level programming?
I have made a custom board with SPC560P40L3, but not able to connect the pls debugger?Please help me with this.Is there any configuration setting need to be changed to connect pls debugger
Thanks @Erwan YVIN , I am able to read,write and erase EEPROM.But , I am able to do it only when it is debug mode.And in Normal rum mode, i am able to read only , but not able to erase and write.Please help me with this.
Thanks @Erwan YVIN . Ya i have one SPC560D-discovery board and through which i am able to program my custom board.But the same custom board i am not able to program using standalone pls debugger.and yes i have checked the pls driver and reinstalled ...
I also have one spc560d discovery board, so i have connected external pls debugger to its 14 pin jtag connector and tap-out the wires from jtag connector also and connected to my custom board.....if the controller of the discovery board is powered O...