2021-04-01 11:42 PM
Hi
In your Reference Manual for the STM32F469 at 31.3.11 it says:
A DMA access is requested when the TXE or RXNE enable bit in the SPIx_CR2 register is
set.
But the SPIx_CR2 Register does not have a TXE/RXNE bit, it has a TXEIE/RXNEIE bit which just en-/disables the Interrupt. Is this a typo or on purpose? The only TXE/RXNE bits I found are in the SPI_SR register...
Solved! Go to Solution.
2021-04-02 04:37 AM
Hello,
The sentence is wrong, and it should be corrected as follow:
“A DMA access is requested when the TXDMAEN or RXDMAEN enable bit in the SPIx_CR2 register is set�?
On my side, I will raise the typo internally for fix.
Thanks for pointing out this error.
Imen
2021-04-02 04:37 AM
Hello,
The sentence is wrong, and it should be corrected as follow:
“A DMA access is requested when the TXDMAEN or RXDMAEN enable bit in the SPIx_CR2 register is set�?
On my side, I will raise the typo internally for fix.
Thanks for pointing out this error.
Imen
2021-04-02 04:41 AM
Thanks for the fix... It just confused me as electronics beginner 😉