cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX Register Callback does not work / is missing for SDADC

Heiko_Gericke
Associate II

Bug Description

STM32CubeMX offers the user an option to register their own callback functions under the advanced settings tab:

Screenshot 2024-04-15 173924.jpg

In this example i have enabled the callback registration for CAN aswell as the SDADC. After generating the code my stm32f3xx_hal_conf.h file looks like this:

 

...

#define  USE_HAL_ADC_REGISTER_CALLBACKS         0U /* ADC register callback disabled       */
#define  USE_HAL_CAN_REGISTER_CALLBACKS         1U /* CAN register callback enabled       */
#define  USE_HAL_COMP_REGISTER_CALLBACKS        0U /* COMP register callback disabled      */
#define  USE_HAL_CEC_REGISTER_CALLBACKS         0U /* CEC register callback disabled       */
#define  USE_HAL_DAC_REGISTER_CALLBACKS         0U /* DAC register callback disabled       */
#define  USE_HAL_SRAM_REGISTER_CALLBACKS        0U /* SRAM register callback disabled      */
#define  USE_HAL_SMBUS_REGISTER_CALLBACKS       0U /* SMBUS register callback disabled     */
#define  USE_HAL_NAND_REGISTER_CALLBACKS        0U /* NAND register callback disabled      */
#define  USE_HAL_NOR_REGISTER_CALLBACKS         0U /* NOR register callback disabled       */
#define  USE_HAL_PCCARD_REGISTER_CALLBACKS      0U /* PCCARD register callback disabled    */
#define  USE_HAL_HRTIM_REGISTER_CALLBACKS       0U /* HRTIM register callback disabled     */
#define  USE_HAL_I2C_REGISTER_CALLBACKS         0U /* I2C register callback disabled       */
#define  USE_HAL_UART_REGISTER_CALLBACKS        0U /* UART register callback disabled      */
#define  USE_HAL_USART_REGISTER_CALLBACKS       0U /* USART register callback disabled     */
#define  USE_HAL_IRDA_REGISTER_CALLBACKS        0U /* IRDA register callback disabled      */
#define  USE_HAL_SMARTCARD_REGISTER_CALLBACKS   0U /* SMARTCARD register callback disabled */
#define  USE_HAL_WWDG_REGISTER_CALLBACKS        0U /* WWDG register callback disabled      */
#define  USE_HAL_OPAMP_REGISTER_CALLBACKS       0U /* OPAMP register callback disabled     */
#define  USE_HAL_RTC_REGISTER_CALLBACKS         0U /* RTC register callback disabled       */
#define  USE_HAL_SPI_REGISTER_CALLBACKS         0U /* SPI register callback disabled       */
#define  USE_HAL_I2S_REGISTER_CALLBACKS         0U /* I2S register callback disabled       */
#define  USE_HAL_TIM_REGISTER_CALLBACKS         0U /* TIM register callback disabled       */
#define  USE_HAL_TSC_REGISTER_CALLBACKS         0U /* TSC register callback disabled       */
#define  USE_HAL_PCD_REGISTER_CALLBACKS         0U /* PCD register callback disabled       */

...

 

As one can see, the define for CAN is correctly set to 1U and is working like expected, but the #define for the SDADC is completely missing.
 
 

Steps to reproduce the issue

I am using STM32CubeMX 6.11.0 with a configured project for the STM32F373CCT6 MCU using the STM32Cube FW_F3 V1.11.4 Firmware Package. I'm currently using STM32CubeIDE 1.14.1. I configured the SDADC peripheral for SDADC1 and SDADC3, both configured as 'Single-Ended zero reference'. After this i enabled the register callback option for SDADC under 'Project Manager>Advanced Settings>Register CallBack'. Then press 'Generate Code'.

Using these steps i can reproduce the code that i added above, where the #define for using the SDADC register callback is completely missing from the stm32f3xx_hal_conf.h file

 

Quick but "dirty" fix

For a quick fix i was able to define USE_HAL_SDADC_REGISTER_CALLBACKS with value 1 as a symbol in CubeIDE under 'Properties>C/C++ General>Paths and Symbols>Symbols' for all configurations and languages, but i hope this will only be a temporary fix.

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hello @Heiko_Gericke ,

 

The issue is reported internally to our team (Internal ticket number: 179076 ) and this will be fixed as soon as possible.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Mahmoud Ben Romdhane
ST Employee

Hello @Heiko_Gericke ,

First let me thank you for posting and welcome to the ST Community.

The request is under investigation, and I will get back to you ASAP.

Thanks.

Mahmoud.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello @Heiko_Gericke ,

 

The issue is reported internally to our team (Internal ticket number: 179076 ) and this will be fixed as soon as possible.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hey Mahmoud,

the quick reply is appreciated. I'm looking forward for this to be fixed.

 

Thanks,

Heiko