2019-11-20 03:14 AM
System Clock is PLL_HSE
HSE connected is 12MHz
HSE_VALUE is set 12000000 & SystemCoreClock = 180000000 in system_stm32f4xx.c
HCLK = 180MHz
PCLK1 = 45MHz
PLLM = 12;
PLLN = 360;
PLLP = RCC_PLLP_DIV2;
PLLQ = 4;
Clocks are configured as expected, cross checked RCC registers through debugger.
Baud rate register is also verified and the value matches with the calculations.
What can be the issue ?
2019-11-20 04:24 AM
Did you have a look with a scope?
2019-11-20 06:04 AM
+1
also, what exactly are "garbage data" - is it reproducible, can you show pairs of transmitted/received characters?
JW
PS Please change your username to a normal nick
2019-11-21 02:18 AM
Here's my code:
int main(void)
{
float tmp_flt = 1.543;
uint32_t apb1Clk;
char tmp_ch = 'A';
char tmp_ch1 = 'B';
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
SystemCoreClockUpdate();
apb1Clk = HAL_RCC_GetPCLK1Freq();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_RTC_Init();
MX_SPI1_Init();
MX_UART5_Init();
/* USER CODE BEGIN 2 */
HAL_Delay(500);
while (1)
{
HAL_Delay(500);
printf("printf float: \n\r");
printf("data on line 2\n\r");
printf("data on line 3\n\r");
HAL_Delay(500);
}
}
printf is used by using following function:
#ifdef __GNUC__
#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)
#else
#define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f)
#endif /* __GNUC__ */
PUTCHAR_PROTOTYPE
{
HAL_UART_Transmit(&huart5, (uint8_t *)&ch, 1, 0xFFFFFFFF);
return ch;
}
Terminal view is as follows:
Kindly go through it, anything else you need just tell me.
Waiting for your valuable input.
2019-11-21 10:42 AM
Very interesting - almost completely repeatable, and much of the characters gets through unaffected, that's remarkable.
I'd say, there's some slight baudrate mismatch involved. I know you are using HSE/crystal and the baudrate is not that high compared to system clock, so the mismatch should be relatively low; but what's on the receiving side? Is it some USB-to-UART converter? Can't that be mismatched? Can you try a different one (different make, different chip)? Or, even better, can you locate a PC with an onboard UART? Can you try to transmit on it and measure precisely enough the bit duration (you need to get to some 1% resolution at least)? Is there some level conversion involved (RS232)?
JW
2019-11-21 08:35 PM
You are right USB to RS232 converter was the issue.
Changed it with FTDI FT232RL.
Now issue is little different as you can see below
and also like below:
Please check
2019-11-21 11:45 PM
I honestly don't know. At this stage, you might really need an oscilloscope or maybe even better a logic analyzer and look at the actual Tx signal.
JW
2019-11-22 12:50 AM
👍