User Activity

Hi all,I'm porting a project from a F072 (Nulceo-F072) to a custom PCB with a STM32L072.The board is going well, except when I try to use the USB (CDC mode).When I plug it into my PC, the OS can see it -         Bus 006 Device 072: ID 0483:5740 STMic...
Hi all,If I recall correctly, CubeIDE V1.8 was very unstable when using the integrated MX, with many of the control components failing to redraw correctly, or not at all. Sometimes you could trick it into drawing by minimising and restoring the form....
Hi all,I have a simple project using a STM32C011J4. Using STM32CubeIDE V1.15. I compile it for both Debug & Release.I program it via STM32Programmer V2.10.The Debug elf file works okay, however, the Release elf does NOT run…Yes! I have checked that t...
Hi,I'm wondering why Option bytes, OTP, and other such regions of Flash are not part of the STM32CubeIDE tool chain?Kind regardsPedro
Hi all,I'm trying to install STM32CubeProgrammer V2.16 on Linux-Suse-Tumbleweed, but I'm having problems:-I have downloaded and unpacked en.stm32cubeprg-lin-v2-16-0.zip (generic linux).user@localhost:~/STMicroelectronics/STM32Cube/STM32CubeProgrammer...