on
2024-05-06
7:00 AM
- edited on
2024-05-07
2:31 AM
by
Laurids_PETERSE
This article includes SPI characteristics and clarification of maximum clock frequency when using PB13 and PB14. They are applicable for STM32H523xx, STM32H533xx, STM32H573, STM32H562xx, and STM32H563xx microcontrollers. The purpose of the article is to anticipate the updates that will occur soon in the “SPI characteristics” tables of the STM32H573xx, STM32H562xx and STM32H563xx datasheets (DS14258 Rev 2 and DS14121 Rev 2).
Unless otherwise specified, the parameters given in the SPI characteristic table are derived from tests performed under the ambient temperature. fPCLKx frequency, and VDD supply voltage conditions are summarized in the datasheet, with the following configuration:
Refer to section “I/O port characteristics” in the STM32H5xx datasheet for more details on the input/output alternate function characteristics (NSS, SCK, MOSI, MISO for SPI).
Note: In the tables below, the terms "master" and "slave" have been replaced respectively by "controller" and "target". This is an intentional change to improve inclusive language, and will eventually be implemented in all documentation.
Table: SPI Characteristics for STM32H573xx, STM32H562xx and STM32H563xx microcontrollers (1*)
Symbol |
Parameter |
Conditions |
Min |
Typ |
Max |
Unit |
fSCK 1/tSCK |
SPI clock frequency |
Controller receiver mode 2.7 V <VDD< 3.6 V |
- |
- |
135/3(2*) |
MHz
|
Controller receiver mode 1.71 V <VDD< 2.7 V |
- |
- |
120/3(2*) |
|||
Controller transmitter mode 2.7 V <VDD< 3.6 V |
- |
- |
135/3(2*) |
|||
Controller transmitter mode 1.71 V <VDD< 3.6 V |
- |
- |
120/3(2*) |
|||
Target receiver mode 1.71 V <VDD< 3.6 V |
- |
- |
120 |
|||
Target transmitter mode 2.7 V <VDD< 3.6 V |
- |
- |
43/6(3*) |
|||
Target transmitter mode 1.71 V <VDD< 2.7 V |
- |
- |
41/6(3*) |
1*. Evaluated by characterization – not tested in production.
2*. When using PB13.
3*. When using PB14.
Table: SPI characteristics for STM32H523xx/STM32H533xx microcontrollers (1*)
Symbol |
Parameter |
Conditions |
Min |
Typ |
Max |
Unit |
fSCK 1/tSCK |
SPI clock frequency |
Controller receiver mode 2.7 V <VDD< 3.6 V |
- |
- |
135/3(2*) |
MHz
|
Controller receiver mode 1.71 V <VDD< 2.7 V |
- |
- |
120/3(2*) |
|||
Controller transmitter mode 2.7 V <VDD< 3.6 V |
- |
- |
135/3(2*) |
|||
Controller transmitter mode 1.71 V <VDD< 2.7 V |
- |
- |
120/3(2*) |
|||
Target receiver mode 1.71 V <VDD< 3.6 V |
- |
- |
120 |
|||
Target transmitter mode 2.7 V <VDD< 3.6 V |
- |
- |
43(3*)/6(4*) |
|||
Target transmitter mode 1.71 V <VDD< 2.7 V |
- |
- |
41.5(3*)/6(4*) |
1*. Evaluated by characterization – not tested in production.
2*. When using PB13.
3*. The maximum frequency in target transmitter mode is determined by the sum of tv(SO) and tsu(MI), which must fit into the SCK low or high phase preceding the SCK sampling edge. This value can be achieved when the SPI communicates with a controller having tsu(MI) = 0 while Duty(SCK) = 50%.
4.* When using PB14.
Consider that PB13 and PB14 are special IOs for UCPD with limited speed (supporting Low speed output and medium speed).
The clock frequency is limited to 3 MHz when PB13 in controller output mode is used.
The clock frequency is limited to 6MHz when PB14 in target output mode is used. In this case, it is the value measured according to the datasheet conditions: IO speed/VDD/Load capacitance.
PB13 impact on controller mode:
PB14 impact on target mode:
Hi @Imen.D ,
The right part of tables are not visible and courtesy of the *** #Khoros javascriptoid, on PC there's no standard bar to shift them to the left.
Why are there no-PB13 lines in those tables for master mode (while there *are* no-PB14 lines for slave mode)?
What do those numbers mean, e.g. what is 135/3MHz, is it meant to be 45MHz?
[EDIT] Okay, now I see, it's 135MHz for all other MOSI pins and 3MHz for PB13.
I'd suggest to split this to several tables, this is quite confusing and will fire back later.
I'd also suggest footnotes for PB13/PB14 at the pin table in DS referring to the SPI characteristics, and I'd also suggest mentioning these rather shocking limitations in the SPI chapter in RM.
Is this limitation of PB13/PB14 restricted to SPI? What about GPIO Output, or any other AF on these pins? [/EDIT]
JW
Hi @waclawek.jan;
Thank you for your valuable feedback.
>> I'd also suggest footnotes for PB13/PB14 at the pin table in DS referring to the SPI characteristics, and I'd also suggest mentioning these rather shocking limitations in the SPI chapter in RM.
Is this limitation of PB13/PB14 restricted to SPI? What about GPIO Output, or any other AF on these pins?
I highlighted your message to trigger a Datasheet update and add this.
Thanks
Imen
Hi @waclawek.jan,
>>The right part of tables are not visible and courtesy of the *** #Khoros javascriptoid, on PC there's no standard bar to shift them to the left.
The tables are fixed.
Thank you again for the continued feedback; it is much appreciated!
Hi @Imen.D ,
well, a maximum from 135 -> 3 MHz is not a tiny difference .
So - why this ?
And what happens, when using a higher frequency on these pins ? chip dies ?
And (as Jan asked ) : Is this limitation of PB13/PB14 restricted to SPI? What about GPIO Output, or any other AF on these pins?