User Activity

Hi I use STM32H743XI and W25Q256 for my design.And I notice W25Q256 has two speed 133Mhz(W25Q256JV) and 104Mhz(W25Q256FV), currently I use W25Q256FV, since I only use this flash with memory map mode, is it necessary to replace with W25Q256JV? Will th...
Hi:I use STM32L4P5RG with APS6404L-3SQR to develop GUI.I want use QSPI PSRAM as data memory for GUI.Now, I enable QSPI PSRAM as data memory as follows:1.configure QSPI PSRAM , SPI with NVIC in CubeMX2. add PSRAM (xrw) : ORIGIN = 0x70000000, LENGTH = ...
Hi :I want to use audio class with AZRTOS, but even I select audio, I still can't find audio in middleware. 
Hi I can't find USB device with MTP example.Is there any resource about USB device with MTP?
Hi I want to improve the FPS of TFT when using SPI interface.I use SPI+DMA+QuadSPI PSRAM+QuadSPI Flash for now.I notice STM32L4P5RG has DMA2D.So can it use for SPI interface?Will it have any improvement when I refresh TFT?If it has, how to use it?
Kudos from
Kudos given to